the MIMXRT1050-EVK uart pin (in the arduino port) is it the UART1 instance ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

the MIMXRT1050-EVK uart pin (in the arduino port) is it the UART1 instance ?

跳至解决方案
3,672 次查看
wassimhammami
Contributor II

Hi,

I have a two MIMXRT1050-EVK boards and I want to communicate between them using UART.

As indicated in the user's guide (picture attached to this post) there is a UART pin in the arduino expansion port, so I want to use it. But I don't know in which instance this pin is attached to ?

(UART1 or UART2 or ...)

Thanks

1 解答
3,452 次查看
art
NXP Employee
NXP Employee

The UART3 port is used in the Arduino interface of the i.MX RT1050 EVK board.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
3,453 次查看
art
NXP Employee
NXP Employee

The UART3 port is used in the Arduino interface of the i.MX RT1050 EVK board.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------