the MIMXRT1050-EVK uart pin (in the arduino port) is it the UART1 instance ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the MIMXRT1050-EVK uart pin (in the arduino port) is it the UART1 instance ?

ソリューションへジャンプ
3,673件の閲覧回数
wassimhammami
Contributor II

Hi,

I have a two MIMXRT1050-EVK boards and I want to communicate between them using UART.

As indicated in the user's guide (picture attached to this post) there is a UART pin in the arduino expansion port, so I want to use it. But I don't know in which instance this pin is attached to ?

(UART1 or UART2 or ...)

Thanks

1 解決策
3,453件の閲覧回数
art
NXP Employee
NXP Employee

The UART3 port is used in the Arduino interface of the i.MX RT1050 EVK board.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
3,454件の閲覧回数
art
NXP Employee
NXP Employee

The UART3 port is used in the Arduino interface of the i.MX RT1050 EVK board.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------