question about the wifi_nxp middleware...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about the wifi_nxp middleware...

Jump to solution
1,772 Views
EdSutter
Senior Contributor II

I am working with the MIMXRT1060EVK and MIMXRT1170EVKB, running with SDK_2_16_000_EVK-MIMXRT1060 and SDK_25_03_00_MIMXRT1170-EVKB.  For both of these boards I am using the same SDIO-based WiFi modem, but I see significant differences between the two directories.

I realize they are different SOCs (1060 vs 1170) but fundamentally the code at the wifi_nxp level should (AFAIK) be the same.  There are significant differences, and it appears to me that the code under the 1170 tree is more mature than that of the 1060 tree.  Can someone explain why they are so different?  Is the 1060 SDK just not as up-to-date as the 1170 tree?

I ask because if it is at all possible, I'd like to not have to use two different source trees for the same WiFi functionality.  

Can someone from NXP support explain this?

  

0 Kudos
Reply
1 Solution
1,709 Views
Sam_Gao
NXP Employee
NXP Employee

Hi,

Please see below comments from my side.

  • Middleware should be same if you use the same version SDK(e.g 25.03) for both RT1060 and RT1170, please check with the same baseline, it should be workable.
  • It is very certain that there has been a major version update from 2.16 to 25.03, the latest one is more mature.

View solution in original post

6 Replies
1,732 Views
EdSutter
Senior Contributor II
Can someone from NXP comment on this?
I guess the question is: can I use the wifi_nxp middleware and work it to run with the iMXRT1060?
0 Kudos
Reply
1,710 Views
Sam_Gao
NXP Employee
NXP Employee

Hi,

Please see below comments from my side.

  • Middleware should be same if you use the same version SDK(e.g 25.03) for both RT1060 and RT1170, please check with the same baseline, it should be workable.
  • It is very certain that there has been a major version update from 2.16 to 25.03, the latest one is more mature.
1,696 Views
EdSutter
Senior Contributor II

@Sam_Gao  I just took a shot at rebuilding my 1060 code (from SDK2.16) with the 1170's (SDK25.03) middleware/wifi_nxp.  I had to make a few small adjustments, but so far (only 10 minutes into my test run), it appears to be working.  So far so good...

Thanks much,

0 Kudos
Reply
1,702 Views
EdSutter
Senior Contributor II

Great news!  Thanks for responding...

So, when I attempt to build the latest SDK for the 1060 (actually for the EVK-MIMXRT1060), the latest available version is 2.16.00. So what is my best approach?  Will the SDK builder somehow build newer versions or should I just attempt to use the wifi_nxp directory from the 1170 when building for the 1060?

Thanks much for responding!!

0 Kudos
Reply
1,665 Views
Sam_Gao
NXP Employee
NXP Employee

Hi,

It depends on actual SW/HW and your requirment.

Yes. It only supports SDK2.16.0 if you select 'RT1060-EVK' board, but you will get a newer version if you have 'RT1060-EVKB'. The SDK version is related to the Hardware.

You can use the latest SDK and port them into the hardware RT1060-EVK. 

0 Kudos
Reply
1,660 Views
EdSutter
Senior Contributor II
Ok, I didn't realize there was a 'B' version for that board. Regardless (referring to my last post), I was able to use the latest wifi_nxp with my older 1060 SDK. Thanks!
0 Kudos
Reply