parallel CSI camera on MIMXRT1170-EVKB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

parallel CSI camera on MIMXRT1170-EVKB

2,616件の閲覧回数
zohargolan
Contributor III

Hi all,
I need to connect a parallel CSI camera to the MIMXRT1170-EVKB using the flexIO. Is there an app note or a project using a parallel camera specifically on the MIMXRT1170-EVKB board? are all the required IOs accessible on the Arduino connectors?
Thank you for your help,
Zohar

0 件の賞賛
返信
4 返答(返信)

2,600件の閲覧回数
zohargolan
Contributor III

Thank you Omar for your reply,

I did saw this application note, but my question was if I can run it on the MIMXRT1170-EVKB board. Do I have all the required IOs going to the Arduino connectors?

 

Zohar

0 件の賞賛
返信

2,561件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

It depends how many pins you need, FlexIO2 only is available on the EVK arduino port on GPIO_AD_00 to GPIO_AD_13 as well as GPIO_AD28 to GPIO_AD31. Please refer to the EVKB schematics.

Best regards,
Omar

0 件の賞賛
返信

2,492件の閲覧回数
zohargolan
Contributor III

Thank you Omar,

It turned out I dont have the pins I need on the Arduino connectors. In order to get to those pins I will have to do heavy rework to the EVK.

I will use the MIPI interface instead (with a custom parallel to MIPI adapter)

 

Zohar

0 件の賞賛
返信

2,606件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this application note: 
Using FlexIO to emulate Parallel Camera Interface on i.MX RT

Best regards,
Omar

0 件の賞賛
返信