loading error for MIMXRT1020 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

loading error for MIMXRT1020 EVK

1,903 Views
bilge_kara157
Contributor II

Hi,there is loading error when I load led_blink or other sample project to i.mx rt1020 evk board on keil uvision 5.24 .Just Hello_world project load.No Algorithm found for: 00000000H - 0000D9BFH.Erase skipped!

Labels (1)
0 Kudos
Reply
1 Reply

1,745 Views
igorpadykov
NXP Employee
NXP Employee

Hi bilge

one can try to download MIMXRT1021_DFP from Keil Pack Installer,

it has MIMXRT1021_QuadSPI_4KB_SEC.FLM (file programming algorithm).

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply