kStatusRomLdrSignature when using MFGTool2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

kStatusRomLdrSignature when using MFGTool2

3,203 次查看
bzhang3
Contributor I

I'm trying to use MFGTool2 to load boot_image.sb onto HyperFlash of the IMXRT1050-EVKB. I followed every step in section 3.4 of the attached AN12107. I repeated multiple times to make sure I did not miss anything. But every time it failed to program the boot image. 

I check the MfgTool.log. It gives me this error:

   "description" : "10101 (0x2775) kStatusRomLdrSignature",

From the reference manual, this error means "ROM SB loader incorrect signature". But I don't know how I got this and what I did wrong. 

Can anybody help please?

Thanks in advance,

Bin

标签 (1)
0 项奖励
回复
2 回复数

3,005 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello Bin Zhang,

What it comes to mind is that the SB file wasn't correctly created, 

did you type in the cmd the correct line,(step 7 in AN12107)? 

elftosb.exe -f kinetis -V -c ../../bd_file/imx10xx/program_flexspinor_image_HyperFlash.bd -o boot_image.sb ivt_flexspi_nor_hello_world_nopadding.bin

Regards, 

Aldo.

0 项奖励
回复

3,005 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hi again, 

I saw your previous threads,

could you tell me if you were able to create the bin file?

Regards,

Aldo.

0 项奖励
回复