iMXRT1170 IDE LinkServer Debug problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1170 IDE LinkServer Debug problem

1,783件の閲覧回数
OmerFY
Contributor I

Hello,

After making the necessary hardware adjustments to use the Octal Flash on the IMXRT1170 EVKB, I started software tests. I made the necessary adjustments with the MCU BootUtility program, uploaded my program code to octal flash and ran it successfully(led blink). Afterwards, I started testing on the MCUXpresso ide. After making the necessary adjustments here (FCB and Flash Driver update), I can successfully load and debug the code on the completely erased (mass-erase) octal flash via the LinkServer debugger. However, when I cut off the power to the EVKB and try to load the code again with the debugger, I get the error "Flash Driver describes no sectors at its base address". But if I do mass erase and try to debug again, I can debug with LinkServer again. Can you help with this? I will insert my nor_flash_config code below. 

 

/*
 * Copyright 2018-2020 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include "evkmimxrt1170_flexspi_nor_config.h"

/* Component ID definition, used by tools. */
#ifndef FSL_COMPONENT_ID
#define FSL_COMPONENT_ID "platform.drivers.xip_board"
#endif

/*******************************************************************************
 * Code
 ******************************************************************************/
#if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1)
#if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__)
__attribute__((section(".boot_hdr.conf"), used))
#elif defined(__ICCARM__)
#pragma location = ".boot_hdr.conf"
#endif

const flexspi_nor_config_t octalflash_config = {
    .memConfig =
        {
            .tag                 = FLEXSPI_CFG_BLK_TAG,
            .version             = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
            .csHoldTime          = 3,
            .csSetupTime         = 3,
            .deviceModeCfgEnable = 1,
            .deviceModeType      = kDeviceConfigCmdType_Spi2Xpi,
            .waitTimeCfgCommands = 1,
            .deviceModeSeq =
                {
                    .seqNum   = 1,
                    .seqId    = 6, /* See Lookup table for more details */
                    .reserved = 0,
                },
            .deviceModeArg = 2, /* Enable OPI DDR mode */
            .controllerMiscOption =
                (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable) | (1u << kFlexSpiMiscOffset_DdrModeEnable),
            .deviceType    = kFlexSpiDeviceType_SerialNOR,
            .sflashPadType = kSerialFlash_8Pads,
            .serialClkFreq = kFlexSpiSerialClk_133MHz,
            .sflashA1Size  = 64ul * 1024u * 1024u,
            .dataValidTime =
                {
                    [0] = {.time_100ps = 16},
                },
            .busyOffset      = 0u,
            .busyBitPolarity = 0u,
            .lookupTable =
                {
                		/* Read */// EEH+11H+32bit addr+20dummy cycles+ 4Bytes read data    //133Mhz 20 dummy=10+10
                		[0 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0xEE, CMD_DDR, FLEXSPI_8PAD, 0x11),//0x871187ee,
                		[0 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, DUMMY_DDR, FLEXSPI_8PAD, 0x0A),//0xb30a8b20,
                		[0 + 2] = FLEXSPI_LUT_SEQ(DUMMY_DDR, FLEXSPI_8PAD, 0x0A, READ_DDR, FLEXSPI_8PAD, 0x04),//0xa704b30a,

						/* Read Status SPI */// SPI 05h+ status data 0X24 maybe 0X04
                		[4*1 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR  , FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x24),//0x24040405,

						/* Read Status OPI *///05H+FAH+ 4byte 00H(addr)+4Byte read
                		[4*2 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0x05, CMD_DDR, FLEXSPI_8PAD, 0xFA),//0x87fa8705,
                		[4*2 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0x00, CMD_DDR, FLEXSPI_8PAD, 0x00),//0x87008700,
                		[4*2 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0x00, CMD_DDR, FLEXSPI_8PAD, 0x00),//0x87008700,
                		[4*2 + 3] = FLEXSPI_LUT_SEQ(READ_DDR  , FLEXSPI_8PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0x00),//0x0000a704,

						/* Write enable SPI *///06h
                		[4*3 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR  , FLEXSPI_1PAD, 0x06, STOP_EXE, FLEXSPI_1PAD, 0x00),//0x00000406,

						/* Write enable OPI *///06h+F9H
                		[4*4 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0x06, CMD_DDR, FLEXSPI_8PAD, 0xF9),//0x87f98706,

						/* Erase sector */ //21H+DEH + 32bit address
                		[4*5 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0x21, CMD_DDR, FLEXSPI_8PAD, 0xDE),//0x87de8721,
                		[4*5 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR  , FLEXSPI_8PAD, 0x20, STOP_EXE, FLEXSPI_1PAD, 0x00),//0x00008b20,

                        /*Write Configuration Register 2 =01, Enable OPI DDR mode*/ //72H +32bit address + CR20x00000000 = 0x01
                		[4*6 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR  , FLEXSPI_1PAD, 0x72, CMD_SDR, FLEXSPI_1PAD, 0x00),//0x04000472,
                		[4*6 + 1] = FLEXSPI_LUT_SEQ(CMD_SDR  , FLEXSPI_1PAD, 0x00, CMD_SDR, FLEXSPI_1PAD, 0x00),//0x04000400,
                		[4*6 + 2] = FLEXSPI_LUT_SEQ(CMD_SDR  , FLEXSPI_1PAD, 0x00, WRITE_SDR, FLEXSPI_1PAD, 0x01),//0x20010400,

						/*block erase*/ //DCH+23H+32bit address
                		[4*8 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0xDC, CMD_DDR, FLEXSPI_8PAD, 0x23),//0x872387dc,
                		[4*8 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, STOP_EXE, FLEXSPI_1PAD, 0x00),//0x00008b20,

						/*page program*/ //12H+EDH+32bit address+ write data 4bytes
                		[4*9 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0x12, CMD_DDR, FLEXSPI_8PAD, 0xED),//0x87ed8712,
                		[4*9 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, WRITE_DDR, FLEXSPI_8PAD, 0x04),//0xa3048b20,

						/* Chip Erase (CE) Sequence *///60H+9FH
                		[4*11 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR  , FLEXSPI_8PAD, 0x60, CMD_DDR, FLEXSPI_8PAD, 0x9F),//0x879f8760,

                },
        },
    .pageSize           = 256u,
    .sectorSize         = 4u * 1024u,
    .blockSize          = 64u * 1024u,
    .isUniformBlockSize = false,
};
#endif /* XIP_BOOT_HEADER_ENABLE 

 

 

 

 

タグ(2)
3 返答(返信)

1,712件の閲覧回数
mayliu1
NXP Employee
NXP Employee

Hi @OmerFY 

 

Thank you for your interest in the NXP MIMXRT product, I would  like to provide service for you.

I think you can refer to this link, this document describe "RT1170 Octal flash enablement"

Please also double check your  cfx file config.

RT1170 Octal flash enablement - NXP Community

mayliu1_1-1735529125828.png

BR

mayliu

0 件の賞賛
返信

1,665件の閲覧回数
OmerFY
Contributor I
Hi @mayliu1,

Thank you for your reply. Yes, I followed this guide and it seems it doesn't help because same problem still occurs.
0 件の賞賛
返信

1,639件の閲覧回数
mayliu1
NXP Employee
NXP Employee

Hi @OmerFY ,

Thanks for your replay and patience.

I think you can use MCU Boot Utility Tool programing MIMXRT1170 successfully.

I suggest you can compare your image generated by MCU Boot Utility Tool with the image generated by MCUXPresso IDE, especially FDCB section.

mayliu1_0-1737108736653.png

For example,  Next Fig is  image generated by MCU Boot Utility Tool. 

mayliu1_1-1737108755859.png

You can use MCUXPresso IDE to generate a hex image.

mayliu1_2-1737108774211.png

Please compare the differences between the two images above, and then modify the evkbmimxrt1170_flexspi_nor_config.c file accordingly, especially lookupTable value.

You can also refer to octal flash chip datasheet to modify your code.

Wish it helps you.
If you still have question about it, please kindly let me know.

 

BR

MayLiu

0 件の賞賛
返信