iMXRT1052 eMMC 5.0 interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1052 eMMC 5.0 interface

2,116 Views
AkshayPatil
Contributor II

Does the iMXRT1052 chipset support or have compatibility with the eMMC 5.0 and 5.1 standard for embedded flash storage (eMMC)?

datasheet syas "Fully compliant with MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.5/4.2/4.3/4.4/4.41/ including high-capacity (size > 2 GB) cards HC MMC. "

0 Kudos
Reply
1 Reply

2,099 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @AkshayPatil,

Technically the RT1052 does support eMMC 5.0 and 5.1, but only because of the fact that these standards are backward compatible. As stated on the following knowledge base article: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/EMMC-5-0-and-EMMC-5-1-work-on-i-MX6/ta-p...

"The EMMC 4.5 or EMMC 5.0 /5.1 is backward-compatible with eMMC4.4, we can use it in eMMC4.4 mode to enable eMMC4.4 functionality and performance" "Booting from a eMMC 4.5 device or high version is not supported, boot ROM will fall back to the eMMC4.4 standard when a eMMC4.5 or high version capable device is detected."

This was written in the context of a i.MX6 platform, but is also applicable to the i.MX RT family.

BR,
Edwin.

0 Kudos
Reply