iMXRT1021 blowing efuse via executable code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1021 blowing efuse via executable code?

ソリューションへジャンプ
3,532件の閲覧回数
t_thurgood
Contributor III

Hi,

We are using the iMXRT1021 and need to blow efuses via executable code.

I have looked at IMXRT1020RM.pdf, but this describes efuse functionality, but not usability. At the moment we can blow efuses either using Blhost/flashloader or MCU Boot Utility/Flashloader.

Is there an application note explaining internal efuse programming?

Can anyone advise how to do this?

I have found a reference to EFUSE_PROG_SUPPLY_GATE which I assume needs to be set, then what?

br,

Tony

1 解決策
3,448件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Tony Thurgood,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to suggest you refer to the ocotp demo which is from the SDK library, this demo demonstrates that uses the KSDK software to access eFuse map.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,448件の閲覧回数
carstengroen
Senior Contributor II

Tony,

perhaps this can be of some help: https://community.nxp.com/thread/492451 

(I assume the same procedure for the 102x ?!)

3,448件の閲覧回数
t_thurgood
Contributor III

Hi Carsten,

Thanks for the link.

I think that is all useful information to get this working for me.

br,

Tony

3,449件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Tony Thurgood,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to suggest you refer to the ocotp demo which is from the SDK library, this demo demonstrates that uses the KSDK software to access eFuse map.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,448件の閲覧回数
t_thurgood
Contributor III

Hi Jeremy,

Thanks for the info.

best regards,

Tony

0 件の賞賛
返信