iMXRT: No Connection with Serial Downloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT: No Connection with Serial Downloader

Jump to solution
7,271 Views
Sam_ECU
Contributor V

Hello,

I've my first custom board with the MIMXRT1062DVJ6B chip and I'm unable to connect to the chip over Serial Downloader and MCUBootUtility.

Sam_ECU_1-1705243750067.png

When "BOOT_MODE_0" is pulled up, my computer recognises there's a connection, but with the error "Unknown USB Device: Descriptor request failed"

Sam_ECU_2-1705243776196.png

My computer has no issue recognising 1060-EVK and 1010-EVK.

The Power, POR_B design is carried over from the 1060-EVK. The board is using the Flash from 1010-EVK (W25Q64JVSSIQ).

Sam_ECU_0-1705243719362.png

Powering and start up appears fine. There was originally an issue with the power supply to NVCC_SD1 but that has been resolved.

I noted that VDD_USB_CAP = 2.36V, but the 1010-EVK is 2.64V.

Sam_ECU_3-1705243816110.png

I've tried to connect with UART as well but there is no connection. I measure 3.33V on UART_TX and UART_RX although in the design they are both open.

What can be the sources for this issue?

Thanks.

 

0 Kudos
Reply
1 Solution
5,973 Views
Sam_ECU
Contributor V

Hello @weidong_sun 

Thanks for the help.

I left the pin floating after the information below in the schematic for the EVK:

Sam_ECU_0-1715799166563.png

Here is the new design:

Sam_ECU_1-1715799199127.png

 

By chance I looked at the datasheet for the common choke (L5 --> L6) and noted that my footprint was wrong and USB_OTG_D- was orientated incorrect.  Pins 3 and 4 were swapped.  I removed the Filter from my board and I can now connect and flash the board over UART using Serial Downloader.

Flashing a program to output "Hello World" over UART1 and to toggle a LED both work, but it hangs up some times and it appears to be related to the clock:

Sam_ECU_2-1715799540376.png

 

If I use the SDK-Example "Hello World" it generates a hardfault,

Sam_ECU_3-1715799921308.png

 

But if I step past the fault then it hangs up just after "armPllConfig_BOARD_BootClockRUN:"

Sam_ECU_4-1715799968070.png

 

Does this mean I have an issue with my 24Mhz XTAL?

I've completed measurements on the XTALO.  Is this acceptable for the device?

Sam_ECU_5-1715800049078.png

 

Regards,

Sam

 

View solution in original post

0 Kudos
Reply
29 Replies
4,111 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @Sam_ECU ,

 

Welcome!

Since the question in the post has been discussed clearly, could you please press "ACCESPT AS SOLUTION" to close the case?

 

Thanks!

Regards,

weidong

0 Kudos
Reply
4,551 Views
youngSheldon
Contributor II

Here's my POR. Basically a simplified version of the EVK schematic for 1010 that takes care of the powerup sequence (R & C values). Serial connection works like a charm.

A few notes though:

  • The board I had problems with was handsoldered so I redesigned it a bit and had a FAB do the assembly
  • I had some issues with a Micron FLASH which I changed.
  • UART works fine. USB is recognized now but I didn't manage to do a programming yet. Sinde UART works, I didn't spend time on it.
  • I am using NXP-MCU Boot Utility which seems to be developed by a NXP employee
  • NXP's support on this was close to zero.

youngSheldon_0-1713883252515.png

 

let it flow
0 Kudos
Reply
4,539 Views
Sam_ECU
Contributor V

Hello @youngSheldon 

Cheers for your input.

Glad you resolved your issues.  I still can't say where my issues lie.

According to the hardware development guide:

Sam_ECU_0-1713896619677.png

And the reference manual:

Sam_ECU_1-1713896660967.png

The power up (measured) fulfills the requirements.

I can also short the POR_B pin to ground during power up and then remove the ground and the issue remains the same, so I'm not convinced the issue lies in POR_B.

Boot_Mode(0) is 3.3V when the POR_B goes high.  Boot_Mode(1) is 0V.

I've no idea, where the issue lies...

0 Kudos
Reply
4,862 Views
anthony_asterisk
Contributor II

I'm having a similar problem, did you find a solution?  @Sam_ECU @nxf77486 

0 Kudos
Reply
4,997 Views
youngSheldon
Contributor II

I'm having a very similar issue with iMXRT1010 on a custom board. I can program the board via JTAG, but when USB is connected the system blocks (looks there is an advice on this in this post).

USB and UART programming both fail. I tested pretty much everything, every single component and connection and I am quite sure there is something in MCU that slips between my fingers. My VDD_USB_CAP is 2V6, same as on EVK.

let it flow
0 Kudos
Reply
5,448 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

Thank you for contacting NXP support.

Can you please help me by trying this configuration on our MCUXpresso Secure Provisioning Tool, also as far as I understand you are booting the application from the RT1010? If this is not the case please let me know.

Regarding voltages I also recommend to give a look into the hardware development guide.

0 Kudos
Reply
5,434 Views
Sam_ECU
Contributor V

Hello @nxf77486 

My board has the MIMXRT1062DVJ6B chip.

There is still no connection when using the Provisioning Tool (USB or UART):

Sam_ECU_0-1705428057691.png

The measured power voltages all conform to those required in the Hardware Manual.

How should I best proceed to determine why's there no communication to the chip on my board?

Thanks,
Sam

0 Kudos
Reply
5,422 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for the information, can you please help me by confirming that the set-up of the pins are set for SD so you can be able to flash the device as you are trying to do.

0 Kudos
Reply
5,412 Views
Sam_ECU
Contributor V

Hello @nxf77486 ,

BOOT_MODE_0 is pulled up to 3.3V.

BOOT_MODE_1 is floating.  I've pulled it down to ground as well but it makes no difference.

0 Kudos
Reply
5,306 Views
Sam_ECU
Contributor V

Hello @nxf77486 

I can flash the chip using MCUXpresso.

I've measured the power up below and referenced it with the information in the "Hardware Development Guide":

Sam_ECU_0-1706122399297.png

BOOT_MODE_0 is connected to F11 with 3.3V. BOOT_MODE_1 ist connected to G14 and floating.

BT_CFG_(x) are all pulled low.

I still can't access the chip over UART or USB in Serial Download mode.

Any and all help appreciated.

Thanks,
Sam

0 Kudos
Reply
5,285 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

I understand thank you for the information.

Can you please help me confirm the LPUART channel you are using, for the serial download you must use the LPUART1.

Please help me verify this.

0 Kudos
Reply
5,246 Views
Sam_ECU
Contributor V

Hello @nxf77486 

Sam_ECU_0-1706614132815.png

Sam_ECU_0-1706614358446.png

 

Sam_ECU_3-1706614241476.png

 

0 Kudos
Reply
5,219 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

I appreciate the information and the image send.

According to the following community post clients that are willing to use the UART it is recommended to unplug USB OTG as this is not allowed can you please he me with this test.

0 Kudos
Reply
5,173 Views
Sam_ECU
Contributor V

Hello @nxf77486 

That's not the issue.

Likewise with no UART attached and only connecting USB

0 Kudos
Reply
4,600 Views
Sam_ECU
Contributor V

Hello @youngSheldon & @anthony_asterisk 

No, I haven't resolved the issue.

I redesigned the board with an update to the POR_B.  I changed the flash to that from the 1060-EVK.

Still the exact same issue.

The help from NXP has been next to useless.

Have you managed to resolve your issues?

Cheers,

Sam

0 Kudos
Reply
4,593 Views
Sam_ECU
Contributor V

My POR_B Design:

Sam_ECU_0-1713806809997.png

 

0 Kudos
Reply
4,585 Views
Sam_ECU
Contributor V

@diego_charles @DanielRuvalcaba 

Could you help me with this issue?

0 Kudos
Reply
4,325 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @Sam_ECU ,

 

It seems that your USB/UART issue has not been resolved yet. 

We can continue to discuss it. 

Would you mind sharing your full schematic with me?

My email is : weidong.sun@nxp.com

Let me check the schematic firstly, then continue to discuss it with you, OK?

 

Thanks!

Regards,

weidong

0 Kudos
Reply
4,313 Views
Sam_ECU
Contributor V

Hello @weidong_sun ,

I sent you an email.  Thanks for looking into the issue.


Regards,

Sam

0 Kudos
Reply
4,298 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @Sam_ECU ,

See below, please!

weidong_sun_0-1715768115102.png

Since you want USB OTG1 to be device mode, ID pin can't be floated, it should be connected to GPIO_AD_B0_01 pin of RT1062, and internal pull-up resistor should be enabled, otherwise external pull-up resistor should be used.

Next, I will check your UART1 circuit.

 

Thanks!

Regards,

weidong

 

0 Kudos
Reply