I wanted to change the UART clock input so the PLL3 could be disabled. So I went ahead and chose PERCLK_CLK_ROOT in the clock tree configurator (MCUXpresso IDE v11.2.1 [Build 4149] [2020-10-07]). It broke all UART connections completely. I had to do a lot of digging to find in the reference manual that this chip has actually a 2-way clock mux (PLL3_SW / 6 or OSC_CLK), there's nothing connected on the 3rd mux input.
This is clearly a bug in the ConfigTools and in the SDK (or in the silicon and in the reference manual), please fix it where appropriate.
已解决! 转到解答。
Hello,
The clock tree in the reference manual is wrong since the perclk is an option for the UART in the RT1010, this will be fixed in future releases of the reference manual.
The SDK example doesn't work when you select this as the clock source because there is a clock gate between the clock root and peripheral, if you enable this gate, you will find the UART can work well. To activate this gate please call the following function in your main before you configure the UART.
CLOCK_EnableClock(kCLOCK_Pit);
Also, there's a problem with the function BOARD_DebugConsoleSrcFreq of the SDK, this function doesn't support the perclk option. This will be fixed in future releases of the SDK as well. In the meanwhile you can change this function manually, it should look like the following:
Regards,
Victor
I'm attaching a quickly generated project:
The result is: the UART console isn't functional, no "Hello world" is printed, the PRINTF call hangs.
Hello @benedek_kupper,
I will make some tests on my end to see if I'm able to replicate the behavior that you mentioned. I will let you know my results as soon as possible.
Regards,
Victor
Hello,
The clock tree in the reference manual is wrong since the perclk is an option for the UART in the RT1010, this will be fixed in future releases of the reference manual.
The SDK example doesn't work when you select this as the clock source because there is a clock gate between the clock root and peripheral, if you enable this gate, you will find the UART can work well. To activate this gate please call the following function in your main before you configure the UART.
CLOCK_EnableClock(kCLOCK_Pit);
Also, there's a problem with the function BOARD_DebugConsoleSrcFreq of the SDK, this function doesn't support the perclk option. This will be fixed in future releases of the SDK as well. In the meanwhile you can change this function manually, it should look like the following:
Regards,
Victor
Hi
I can confirm the same findings using the configuration that I prepared for the uTasker project.
Your printf() is probably using a blocking method if it hangs since the LPUART just does nothing and doesn't cause a failure in accessing it, etc.
Therefore PLL3_SW/6 is fine and OSC_CLK is fine but when trying to use PER_CLK the LPUARTs don't respond.
What I can say is that if the clock path is set back from the PER_CLK setting to one of the two that operate the LPUART starts working again - with the PER_CLK source setting my interrupt driven LPUART driver doesn't get any interrupts and so has data in its SW queue waiting to be transmitted. As soon as the clock is changed the interrupts start arriving and the data then goes out.
Therefore this new switch setting looks to be a red-herring that the config tools developers also used without testing it.It looks more like the register description is wrong but the clock diagram in right. The question is where did this new register description come from? Was it a mistake or was it actually envisaged that the i.MX RT 1011 would have this additional option at some point but it was forgotten, or it has a silicon errata?
The mystery continues !!!
In any case, as you presumably have done, using OSC_CLK allows PLL3 to be disabled if not used by any other parts of the system.
Regards
Mark
Hi
Attached is a binary that shows the situation on the iMX RT 1010 EVK. Here is how it can be used:
1. Load using MCU Boot Utility or whatever binary loader is available
2. It tries to send a welcome message to the LPUART (115 kBaud) but nothing comes out
3. The board enumerates as USB-CDC on the processor's HS-USB and when connected to a terminal emulator a command line menu is available. Hit 'Enter' to see it and then '3' to enter the I/O menu
4. Check the CCM_CSCDR1 register value with
""md 400fc024 l 1" which will show that the switch is set as wanted (0x00000080 bit set)
5. Change the value back to PLL3/6 with
"mm 400fc024 l 06000006"
or to OSC_CLK with
"mm 400fc024 l 06000046"
At this point the queued welcome message is sent out over the LPUART (although not with the correct baud rate due to the different baud clock speed.
Regards
Mark
USB-CDC terminal session reference:
Serial number: 00
Software version V1.4.014
Device identification: uTasker Number 1
Main menu
===================
1 Configure LAN interface
2 Configure serial interface
3 Go to I/O menu
4 Go to administration menu
5 Go to overview/statistics menu
6 Go to USB menu
7 Go to I2C menu
8 Go to utFAT disk interface
9 FTP/TELNET commands
a CAN commands
help Display menu specific help
quit Leave command mode
3
Input/Output menu
===================
up go to main menu
md Memory Display [address] [<l>|<w>|<b>] [num]
mm Memory Modify [address] [<l>|<w>|<b>] [val]
mf Memory Fill [address] [<l>|<w>|<b>] [val] [num]
sd Storage Display {as md}
sm Storage Modify {as mm}
sf Storage Fill {as mf}
se Storage Erase [address] [len-hex]
sr Status read
sw Status write
set_ddr Set port type [1..4] [<i>|<o>
get_ddr Get data direction [1..4]
read_port Read port input [1..4]
write_port Set port output [1..4] [0/1]
out output value [hex]
save Save port setting as default
help Display menu specific help
quit Leave command mode
#md 400fc024 l 1
Memory Display
0x400fc024 06000086 ....
#mm 400fc024 l 06000006
Write - OK
#
Hello,
The UART in the RT1011 does have three different clock source options, you can see this in the register CCM_CSCDR1 under the UART_CLK_SEL field. There is a problem with Figure 14-3 of the reference manual because in this clock tree we don't mention the per_clk_root, I already reported this to the documentation team so they can fix it in future releases.
Regards,
Victor
Hi
Thanks for that useful information, which I didn't know before.
I just updated the uTasker user's guide https://www.utasker.com/docs/iMX/i.MX_RT_1011_uTasker.pdf and driver in order to use this setup too.
Regards
Mark
Hi
Such an error will not be restricted to the 1011 since the LPUART clock is the same in all i.MX RT 10XX parts.
From the uTasker developer's practical guide: https://www.utasker.com/docs/iMX/i.MX_RT_1021_uTasker.pdf (1011 guide points to this one for the UART clock since it is globally the same) these are the two possibilities:
The guides are available for a complete list of all clocking possibilities to more easily visualise the capabilities and restrictions.
As noted, there is in fact a third configuration of 4MHz when PLL3 disabled (but bypassed) but it is not a very interesting method.
Maybe the config tool is trying to do this but forgets to bypass the PLL? Or you have manually changed the bypass setting in the process of disabling the PLL?
Regards
Mark