iMX-RT RAM requirement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX-RT RAM requirement

1,753件の閲覧回数
vinayakaghor13
Contributor I

Hello,

I want to know if I use FRAM instead of SDRAM, then which functions I will not be able to use for IMX RT 1052

Regards,

Vinayak

ラベル(1)
0 件の賞賛
返信
1 返信

1,658件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinayak

if FRAM timings are the same as SDRAM, there are no restrictions for IMX RT1052,

except probably FRAM life time.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信