i.mx rt1050 booting from LPSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx rt1050 booting from LPSPI

ソリューションへジャンプ
2,601件の閲覧回数
christiangradl
Contributor III

What are the exact bootmode/pins settings for booting via LPSPI?

in the TRM table 8-8 there is no entry about this.

Above there stands

   The chip supports these boot flash devices

       Serial NOR/EEPROM boot via LPSPI

ラベル(1)
1 解決策
2,261件の閲覧回数
christiangradl
Contributor III

OK, thanx, that info helps.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,261件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Christian

pinmux settings are given in Table 8-1. ROM Bootloader Peripheral PinMux
i.MX RT1050 Processor Reference Manual

Boot mode only using fuse mode as shows Table 8-35 (there is no GPIO override mode),
fuse selections are given in Table 5-9. Fusemap Descriptions i.MX RT1050 Processor
Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,261件の閲覧回数
christiangradl
Contributor III

Hi

in table 5-9 there is no definition for booting woth LPSPI. Register 0x450[7:0]???

I can select the LPSPI chipselect register 0x6D0, but how can i select the boot device for LPSPI,

as described in chapter 8-2

    The boot ROM supports these boot devices:
   • Serial NOR Flash via FlexSPI
   • Serial NAND Flash via FlexSPI
   • Parallel NOR Flash via SEMC
   • RAWNAND Flash via SEMC
   • SD/MMC
   • SPI NOR/EEPROM via LPSPI

0 件の賞賛
返信
2,261件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

boot ROM uses it as recovery device using one of the LPSPI ports,

please check description in sect.8.10 Recovery devices

Best regards
igor

0 件の賞賛
返信
2,262件の閲覧回数
christiangradl
Contributor III

OK, thanx, that info helps.

0 件の賞賛
返信