i.mx RT1020 Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx RT1020 Problem

1,527 Views
mustafa_tarhan
Contributor II

Hi

When any UART input is high at the powering up stage of the IMXRT1020, seems that the MCU cannot run properly (we cannot see 1.1V supplied by the MCU and nothing works). We observed that issue for these cases:

- When an active (means it drives its tx pin high) UART/RS232 converter is connected to UART1 (debug console) of IMXRT1020

- When we connect RS485 converter to UART2 of IMXRT1020 and the converter drivers rx pin as high

When we isolate those pins, MCU runs perfectly, but when any of them is connected while powering up the MCU, MCU does not work.

We haven't specifically tested all other interfaces, if they have also similar problems. Our problem is on these UART interfaces for now.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,455 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mustafa TARHAN ,

   This question is the same question in your case 00239039.

   After several round reply, I think you can let our customer check the power up sequence, whether it is the same as this figure:

pastedImage_1.png

Any updated information, you can reply me in the case or here.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply