i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled

跳至解决方案
1,500 次查看
SeenFan
Contributor II

Trying to enable SSC on RT1170 EVK with MCUXpresso.

Ref: AN12879

Steps:

1. Base project: SDK Example evkmimxrt1170_semc_cm7

2. Using IDE to config SSC 

IDE_Clocking.png

source_diff.png

3. Boot failed

Boot_Failed.png

4. Sometimes can boot normally (~ 1/50)

Any step I missed?

Regards

Seen

0 项奖励
回复
1 解答
1,439 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @SeenFan ,

This is because RT1170 FlexSPI use PLL2 as clock source when use default configure. When you change PLL2 frequency, FlexSPI may fail to get next instruction. To resolve this, you can put fsl_clock.c to SRAM. Please refer to my demo code.

 

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,440 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @SeenFan ,

This is because RT1170 FlexSPI use PLL2 as clock source when use default configure. When you change PLL2 frequency, FlexSPI may fail to get next instruction. To resolve this, you can put fsl_clock.c to SRAM. Please refer to my demo code.

 

Regards,

Jing

0 项奖励
回复
1,414 次查看
SeenFan
Contributor II

Hi Jin,

If I want to locate and run program on SDRAM. 
What I need to pay attention to?

 

Regards

Seen

0 项奖励
回复
1,406 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @SeenFan ,

SDRAM can be initialized by DCD and boot ROM.  Then boot ROM will copy your application code to SDRAM. I think the most important thing is the cache problem. You can refer to these link.

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-move-CM4-core-project-to-SDRAM-in-RT1176...
2.debug in sdram
https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/m-p/1405167
3.Using NonCached Memory on i.MXRT
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369

Regards,

Jing

 

0 项奖励
回复
1,421 次查看
SeenFan
Contributor II

Hi Jing,

It works. Thanks a lot.

 

Regards

Seen

0 项奖励
回复