i.MX RT Boot Loading Concept Video

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT Boot Loading Concept Video

1,976 Views
mjbcswitzerland
Specialist V

Hi All

I am pleased to present a general i.MX RT boot loading concept that has been finalised in the uTasker project to allow:
- IP and clone protection with AES256 level security without the need to configure for BEE on-the-fly encryption
- serial loaders with various capabilities - all AES256 encrypted (USB device [MSD, KBOOT], USB host (memory stick), SD card, UART Kboot, SREC, iHEX, Ethernet, Modbus
- Integrated secure OTA (Over-The-Air) capability with intermediate storage to memory stick, SD card or QSPI flash

Video discussing and demonstrating the concept on i.MX RT 1062 (concept compatible on i.MX RT 1011 though to i.MX RT 1064):

https://youtu.be/2XfgZq19XDw

The boot loader flow diagram can be viewed at https://www.utasker.com/docs/iMX/Loader.pdf
and the uTasker serial loader's guide at https://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf

This makes high security and flexible boot loading/OTA child's play for professional projects, with no development time needing to be lost. Videos to follow will show how simple it is to configure for any i.MX RT parts and build with MCUXpresso, IAR and GCC make file.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

Labels (4)
0 Kudos
Reply
1 Reply

1,835 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mark Butcher,

Thanks for your reply.

BR,

Jeremy

0 Kudos
Reply