i.MX RT 1064 IAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT 1064 IAP

2,883 Views
zhangyanming
Contributor I

Lately,i use i.MX RT 1064 to develope a product,i want to ask when i update my code,how i use the IAP to update the code in the 4MB Flash on-chip,is there any example? 

0 Kudos
Reply
2 Replies

2,484 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the information as the link  https://community.nxp.com/thread/481446  .Hope it help you.

0 Kudos
Reply

2,484 Views
zhangyanming
Contributor I

i.MX RT 1064 is different from i.MX RT 1052.The i.MX RT 1064 processor contains 4 MB on-chip flash,and the ROM bootloader provides a set of ROM APIs to simply the In-Application Programming (IAP),but i do not find any example in the SDK about the IAP function.i want to find some examples about the ROM APIs,especially the function about  FLASH API.
 

0 Kudos
Reply