example code for multiple ADC CHANNELS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

example code for multiple ADC CHANNELS

1,838 Views
jagadeesh_11
Contributor I

Hi,

i am using rt1050 EVKB board. i am able to read the voltage from single channel ADC1 channel 0.

i want to use another four channels. please help me with an example code.

Regards,

jagadeesh

 

0 Kudos
Reply
1 Reply

1,829 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) I want to use another four channels. please help me with an example code.
-- To provide the fastest possible support, I'd highly recommend you to refer to the adc_etc demo in the SDK library, the demo illustrates how to use the ADC-ETC module to sample multiple ADC pins in order.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply