camera for RT1050 EVKB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

camera for RT1050 EVKB

1,588 次查看
jagadeesh_11
Contributor I

Hi,

can anyone suggest a camera module for RT1050 EVKB which is actively Available with a maximum length of cable.

Regards,

Jagadeesh s

0 项奖励
回复
2 回复数

1,576 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Jagadeesh,

We can suggest MT9M114 module that is the one we use in our SDK examples.

https://www.nxp.com/docs/en/application-note/AN12110.pdf

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 项奖励
回复

1,538 次查看
jagadeesh_11
Contributor I

Hi,

What is the Maximum length of the cable between camera module and the evaluation Board RT1050.

Please provide us the link to buy online.

Best Regards,

jagadeesh 

0 项奖励
回复