boot problem rt1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

boot problem rt1064

2,181件の閲覧回数
tomerk
Contributor I

Hello,
I have a problem with the internal flash boot,

When i load it with the debugger everything works fine but without it the CPU wont begin running.

The legs are set

boot_mode1= 1,

boot_mode0=0

and all the boot_cfg to 0 

what could be the issue?

0 件の賞賛
返信
4 返答(返信)

2,164件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @tomerk ,

Thanks for your interest in NXP I.MXRT series.

Can you help clarify here? What do you mean the CPU won't run when debugger is not used?

Thanks!

 

Best regards,

Gavin

0 件の賞賛
返信

2,139件の閲覧回数
tomerk
Contributor I

some of the times when i give power nothing happens. In some cases the circuit turns on but probably goes straight into BOOT (one of the lights on the circuit lights up for me).  Only in this mode can I burn it and run the mcuxpresso DEBUGGER and then through the DEBUGGER it runs. As soon as I turn off the power and turn it back on, it returns to the states I wrote down. 

0 件の賞賛
返信

2,100件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @tomerk ,

Hope you are doing well!

In your description it seems that image is flashed into RAM to run? Suggest you try deleting and re-importing one of the simplest demos: e.g. Hello_world. Also, switch to 5V DC_DC power supply.

1. make sure SW7 is 0-0-1-0;
2. connect the jumper on J1 to 1-2 pin; (at this time the power supply is the 5V from the J1 port)
3. adjust SW1 to turn on the power supply switch;
4. flash IMAGE through J41;

Best regards,
Gavin

0 件の賞賛
返信

2,092件の閲覧回数
tomerk
Contributor I

Hi, thanks for the response, 

I'm using the module only and not the evk.

0 件の賞賛
返信