Yocto support for iMXRT1180 Crossover MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto support for iMXRT1180 Crossover MCU

Jump to solution
1,046 Views
vilas_shetty
Contributor III

Hello

I am trying to find out whether iMXRT1182 processor will support yocto Linux. I am developing a project which requires OS support. Can anyone help me out in this. How can i get started with iMXRT1182 MCU.

 

 

0 Kudos
Reply
1 Solution
992 Views
samsaprunoff
Contributor V

Good day,

The RT processors support a number of OS's:

- Zephyr  (which was created/modelled after Linux if I recall)

- FreeRTOS

- uTasker

- Nuttx (https://nuttx.apache.org/)

There are probably others, but these are a few that come to mind. 

Cheers,

Sam

 

 

 

View solution in original post

0 Kudos
Reply
5 Replies
973 Views
vilas_shetty
Contributor III

Thank you Pavel Hernandez and samsaprunoff 

 

1,021 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, however the RT1180 is a Cross MCU and does not have support for OS, if you want to use a Linux system, I recommend review the IMX6 or IMX8.

i.MX 8 Series Applications Processors | Arm® Cortex®-A72/A53/A35/M4 cores | NXP Semiconductors

i.MX 6 Series Applications Processors | Multicore Arm Cortex-A7/A9/M4 | NXP Semiconductors

Best regards,
Pavel

0 Kudos
Reply
1,012 Views
vilas_shetty
Contributor III
Hello Pavel Hernandez, Thank you for your response.
Well it means i wont be able to have any os into iMXRT series of MCU. Then how these MCU's are setup. it it only with bare metal or it can support RTOS too?
0 Kudos
Reply
993 Views
samsaprunoff
Contributor V

Good day,

The RT processors support a number of OS's:

- Zephyr  (which was created/modelled after Linux if I recall)

- FreeRTOS

- uTasker

- Nuttx (https://nuttx.apache.org/)

There are probably others, but these are a few that come to mind. 

Cheers,

Sam

 

 

 

0 Kudos
Reply
1,000 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, yes this can be programed as bare metal or using the HAL library from NXP available on the examples SDK and yes is compatible with RTOS.

Best regards,
Pavel

0 Kudos
Reply