The RT1050 has a revision A1/B, and consequently there is a RT1050-EVKB eval board.
Will there be a new revision of the RT1020 (and RT1020-EVK)?
Hello,
There are no plans for future releases of the RT1020.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks Victor. Should the RT1020 be considered as end-of-life?
Hello,
No, the longevity program of the RT1020 is 15 years.
Regards,
Victor