Wifi - how to enable 802.11e (QoS)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wifi - how to enable 802.11e (QoS)

ソリューションへジャンプ
1,792件の閲覧回数
h_bouchard
Contributor III

Hello,

We are using the PAN9026 module along with NXP SDK 2.9.1.

We are transferring voice data over WiFi and would like to enable the 802.11e protocol. I know that PAN9026 supports it. I can see that LWIP also supports this. However, I don't see how to enable it in the PAN9026 using Wifi module of NXP SDK. I see a lot of IOCTL functions in mlan_ioctl.h and other functions in mlan_glue.c but I don't know which one (if any) to use.

Can someone help?

Regards,
Hugo

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,773件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @h_bouchard,

Unfortunately, the only device right now that supports WMM is the 88W8987 but there's been some major changes in the Wi-Fi SDK since the 2.9.1, the latest one is the 2.11.1 and there's been changes between these two versions that could improve the performance.

BR,

Alexis Andalon

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,774件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @h_bouchard,

Unfortunately, the only device right now that supports WMM is the 88W8987 but there's been some major changes in the Wi-Fi SDK since the 2.9.1, the latest one is the 2.11.1 and there's been changes between these two versions that could improve the performance.

BR,

Alexis Andalon

0 件の賞賛
返信