Use IS25LP064D for booting RT1172

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use IS25LP064D for booting RT1172

215件の閲覧回数
jaimy_v
Contributor I

We are planning to use a custom board with RT1172 and connect IS25LP064D on FlexSPIA.  Do we need to change the MIMXRT1170_SFDP_QSPI.cfx for booting from IS25LP064D in MCUXpresso IDE? We are planning to use JLink for code download and debugging. Is the flexspi_nor_config_t qspiflash_config available for  IS25LP064D ?

0 件の賞賛
返信
2 返答(返信)

187件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Hi,

Please refer to this related post and have a try. The flash driver config should be done fisrtly.

0 件の賞賛
返信

112件の閲覧回数
jaimy_v
Contributor I

Thank you, we will refer the flash configuration mentioned in post. But when using Jlink should we change the MIMXRT1170_SFDP_QSPI.cfx in MCUXpresso IDE. In my understanding this is used only when we use Link server. When we debug with JLINK and try to debug the code from flash should we make any other changes.

0 件の賞賛
返信