USB does not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB does not work

1,976件の閲覧回数
glebkit
Contributor I

Good day.

We have faced with problem that USB1 on RT1051 does nit work.

All power supplies are well (USB CAP, USB VDD and other digital supplies).

USB even does not work in full speed (thus the trouble is not in DP/DM layout).

The MCU is stalling after command execution

static void USB_DeviceEhciSetDefaultState(usb_device_ehci_state_struct_t *ehciState){

...

hciState->registerBase->DEVICEADDR = 0U;

}

Also USB bootloader does not work.

What bug can cause all these problems?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,841件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Please try to verify 24 MHz (XTALI/XTALO) oscillator frequency,  which

inaccuracy \ stability is USB sensitive. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,841件の閲覧回数
glebkit
Contributor I

Good day.

We have verified it already.

We even soldered quartz 24 MHz from EVK.

No changes

0 件の賞賛
返信