We previously designed a custom board using MIMXRT1064DVL6A, which is the 10x10 mm package. Now that the 12x12 mm package is available, we would like to use that instead. Besides package size, are there any other differences between them? We have reviewed datasheet and manual and cannot find any differences, but want to double-check.
Regards,
Jason
已解决! 转到解答。
Hi Jason,
You are correct, there are no differences apart from the package.
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored.
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------
Hi Jason,
You are correct, there are no differences apart from the package.
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored.
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------