USB CDC-ECM Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB CDC-ECM Support

5,049件の閲覧回数
w2vy
Contributor V

In the Device Stack Reference I see mention of CDC ACM and CDC RNDIS (and RNDIS is build upon ACM)

In the Host Stack Reference the CDC description seems to be more generic.

I need to support CDC-ECM on the USB Host of the RT1050, is the host side typically a thin layer between the USB and a virtual Ethernet Interface on the IP Stack?

I don't expect to be able to support RNDIS since my host does not support the Microsoft NDIS protocol.

While less important, CDC-ECM Device support would be nice to have too.

Tom

0 件の賞賛
返信
1 返信

4,364件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Tom,

On the MCUXpresso SDK v2.4.0 for EVKB-MIMXRT1050, it is available an CDC Host example under “usb_examples->host_cdc_bm”. This example asks for a USB-UART Device, so, it will be required applying the proper changes to work with USB-Ethernet and with the desired functionality.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信