Hi all,
I'm learning how to use FreeRTOS on the IMXRT1050 and I'm having trouble sending a message on a Queue from an ISR. I'm the pushbutton on the IMXRT1050-EVKB and the gpio input interrupt sample code.
When I set a flag in the ISR, read the flag in a task, then call xQueueSend() from the task it works okay.
However when I try to use xQueueSendFromISR() I get stuck on line 782 of port.c.
configASSERT( ucCurrentPriority >= ucMaxSysCallPriority );
ucCurrentPriority is 0 and ucMaxSysCallPriority is 32.
I'm kind of lost as to what to do. I tried setting NVIC_SetPriority(EXAMPLE_SW_IRQ, 32U); but that didn't help.
Any suggestions?
My code:
void EXAMPLE_GPIO_IRQHandler(void)
{
/* clear the interrupt status */
GPIO_PortClearInterruptFlags(EXAMPLE_SW_GPIO, 1U << EXAMPLE_SW_GPIO_PIN);
/* Change state of switch. */
g_InputSignal = true;// PRINTF("Pushbutton ISR");
xQueueSendFromISR(publish_queue, &event, NULL);
/* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store immediate overlapping
exception return operation might vector to incorrect interrupt */
#if defined __CORTEX_M && (__CORTEX_M == 4U)
__DSB();
#endif
}void gpio_init(void)
{
/* Define the init structure for the input switch pin */
gpio_pin_config_t sw_config = {
kGPIO_DigitalInput,
0,
kGPIO_IntRisingEdge,
};
/* Init input switch GPIO. */
// NVIC_SetPriority(EXAMPLE_SW_IRQ, 32U);
EnableIRQ(EXAMPLE_SW_IRQ);
GPIO_PinInit(EXAMPLE_SW_GPIO, EXAMPLE_SW_GPIO_PIN, &sw_config);/* Enable GPIO pin interrupt */
GPIO_PortEnableInterrupts(EXAMPLE_SW_GPIO, 1U << EXAMPLE_SW_GPIO_PIN);publish_queue = broker_register_publisher(topic);
if (xTaskCreateStatic(gpio_task, "gpio_task", GPIO_TASK_STACK_SIZE, NULL, GPIO_TASK_PRIORITY, gpio_task_stack, &gpio_task_buffer) == NULL)
{
PRINTF("Task creation failed!.\r\n");
while (1)
;
}
}void gpio_task(void *pvParameters)
{
while (1)
{
if (g_InputSignal)
{
delay();
if (1 == GPIO_PinRead(EXAMPLE_SW_GPIO, EXAMPLE_SW_GPIO_PIN))
{
// PRINTF("Sending Pushbutton\r\n");
// xQueueSend(publish_queue, &event, 0);
}/* Reset state of switch. */
g_InputSignal = false;
taskYIELD();
}
}
}static void delay(void)
{
volatile uint32_t i = 0;
for (i = 0; i < 1000000; ++i)
{
__NOP(); /* delay */
}
}
解決済! 解決策の投稿を見る。
I have a piece of code I paste in whenever I'm about to enable an interrupt. From memory, it looks like:
> NVIC_SetPriority(xxx_IRQn, configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY);
That second argument isn't the value being compared -- that's configMAX_SYSCALL_INTERRUPT_PRIORITY, which is what the CPU actually works with. Your choice of 32 is probably too large, since __NVIC_PRIO_BITS is 4 in the RT1015.
Hi Bruce,
Okay setting the priority to 4 seemed to get the interrupt to work.That's the priority of my tasks.
I put a breakpoint on the line that was crashing before and my ucCurrentPriority came out as 64. I don't really understand the relationship between my ISR priority and the priority that appears in that port.c function but that's a problem for another day.
Thanks.
I have a piece of code I paste in whenever I'm about to enable an interrupt. From memory, it looks like:
> NVIC_SetPriority(xxx_IRQn, configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY);
That second argument isn't the value being compared -- that's configMAX_SYSCALL_INTERRUPT_PRIORITY, which is what the CPU actually works with. Your choice of 32 is probably too large, since __NVIC_PRIO_BITS is 4 in the RT1015.