Switch from VDD_HIGH_IN to VDD_SNVS_IN of RT family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Switch from VDD_HIGH_IN to VDD_SNVS_IN of RT family

Jump to solution
1,788 Views
fredfu
NXP Employee
NXP Employee

Hi,

      In RT1052 RM, there is a bit to control switch from VDD_HIGH_IN to VDD_SNVS_IN, could you help to provide detailed description of the controlling circuit?

   Capture.PNG

Best Regards,

Fred Fu

0 Kudos
Reply
1 Solution
1,778 Views
wayne_wang
NXP Employee
NXP Employee

it can be disabled only when VDD_SNVS_IN and VDD_HIGH_IN both powered.

View solution in original post

0 Kudos
Reply
3 Replies
1,785 Views
wayne_wang
NXP Employee
NXP Employee

there is a internal diode between VDD_HIGH_IN and VDD_SNVS_IN, and this switch has function only in VDD_HIGH_IN and VDD_SNVS_IN powered, otherwise, it will always enable.

0 Kudos
Reply
1,780 Views
fredfu
NXP Employee
NXP Employee

Hi  Wayne,

    Thanks. Can the switch be disabled? if customer don't need the channel from VDD_HIGH_IN to VDD_SNVS_IN.

Best Regards,

Fred Fu

0 Kudos
Reply
1,779 Views
wayne_wang
NXP Employee
NXP Employee

it can be disabled only when VDD_SNVS_IN and VDD_HIGH_IN both powered.

0 Kudos
Reply