Hi fengxingsheng,
You are from China, so you can read this document which will be useful to you, this document is written by our AE, the MCUBootutility author:
https://www.cnblogs.com/henjay724/p/12098657.html
• Integrated I-TCM and D-TCM RAM controller
• 64-bit I-TCM interface and 2x 32-bit D-TCM interface.
• Synchronous interface to the M7 Core,run at the same frequency as the core
• Integrated OCRAM controller
• As slave module on the 64-bit system AXI bus
• Synchronous to the system bus, runs at the same frequency as bus fabric

Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------