Hello Alistair Lowe,
- Does Zephyr work alongside HAB for secure booting? (i.e. does mcuboot support HAB), if not, is this on the roadmap? If so, where can I find documentation?
Yes, Zephyr works alongside with HAB for secure booting. You can request the download of the application note, How to use HAB secure boot in i.MX RT10xx in the following link. Additional to that, the following community document gives a detailed analysis of how HAB works, RT1050 HAB Encrypted Image Generation and Analysis.
- Does Zephyr make use of any of the hardware encryption and other security features of the i.MX RT range?
For this question, it will be necessary to contact Zephyr directly.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------