Setting PWM signal level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting PWM signal level

ソリューションへジャンプ
1,595件の閲覧回数
Gamka
Contributor III

I am using imxrt1064 and the pwm example as a starting point. I can setup the PWM duty cycle and frequency. The PWM signal is always 3V/0V. Is there a ways to setup the PWM signal level to e.g. 0.4V?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,587件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Gamka,

The PWM module has several features that are describes in the Reference Manual, but it has a fixed voltage level to the same level as the GPIO signals.

My apologies for the inconvenience.

Regards,
Gustavo

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,578件の閲覧回数
Gamka
Contributor III

Could the PWM signal be somehow routed to some DAC and then set the DAC value? I just realized, that apparently there is no DAC in imxrt1064... So I guess no.

Br, Kaisa

0 件の賞賛
返信
1,588件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Gamka,

The PWM module has several features that are describes in the Reference Manual, but it has a fixed voltage level to the same level as the GPIO signals.

My apologies for the inconvenience.

Regards,
Gustavo

0 件の賞賛
返信