Setting MCU-Link COM Port configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting MCU-Link COM Port configuration

4,324 次查看
scornelius
Contributor III

I've been using the LPC-Link 2 and MCUXpresso running on Windows 10.
I am now looking at the MCU-link.
Using device manager, when trying to configure the VCOM, I have two related questions.
From within device manager, after selecting "Properties":

  1. How do I set the "Bits per second"?
    For the LPC-Link2 this is under a "Port Settings" tab.

  2. Similarly, how do I set the COM port?
    For the LPC-Link2 this is under a "Port Settings" tab, then the "Advanced..." button, and then "COM Port Number".

I looked under the "Details" tab but didn't see any related settings.

Thanks for any guidance.

0 项奖励
回复
6 回复数

4,312 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Yes, it missing the Porting setting as it uses the NXP's own driver instead of Microsoft.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

4,306 次查看
scornelius
Contributor III

Thank you for the prompt reply, but I think that this deficiency needs to be escalated.
It's good to know that NXP owns the driver, and can maintain the quality.

The "Port Settings" tab is not only available in Microsoft driver.
The drivers from other vendors (mbed, Prolific, etc) have the tab.

When using multiple debug adapters with multiple boards, it's useful that the COM ports do not move around. I have multiple boards (custom, and EVKs) connected at once.

Another issue: the driver improperly selected COM4, a port that was previously assigned, but not active.
When I activated it (via USB HUB switch), the original device could not start because of the overlap.
You can see that problem below.

scornelius_2-1621342521016.png

I tried uninstalling the MCU-Link on COM4. When I cycled it's power, it returned to COM4, this time overlapping the active COM4 device.

Is there any possibility NXP's driver can be corrected to fix this selection problem?
And possibly add the "Port Setting"?

Thanks again

0 项奖励
回复

4,294 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Is there any possibility NXP's driver can be corrected to fix this selection problem? And possibly add the "Port Setting"?
-- I'll report the phenomenon to the AE team for further checking later.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

4,284 次查看
scornelius
Contributor III

I appreciate you passing this on.
I'll hope for their reply.

Thank you very much,
  SWC

0 项奖励
回复

4,255 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
According to the reply of the MCU-Link team, they were able to confirm that the missing Port Settings tab in the device managers properties is an oversight of the MCU-Link VCOM driver.
And they will fix the bug in a subsequent MCU-Link firmware update utility package (which includes and installs the necessary device drivers on Windows).
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

4,236 次查看
scornelius
Contributor III

That's good to hear!
Looking forward to the driver update.

Thanks for the follow through,
  Steve

0 项奖励
回复