Serial manager - multiple interfaces

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial manager - multiple interfaces

1,506 Views
kl
Contributor III

Hi.

I have a application for a custom board, and it runs fine with serial_manager for fsl_debug_console or fsl_shell. 

But If I register both the USB and the UART Debug Console only the last one registered is actually active. 

Is this intentional? All the code for serial manager is build very modular, so It should not be a big task to allow dual debug/shell interface.

Am I the only one with this requirement?

I have a plan implementing a interface for a network/telnet to the Serial Manager, but if serial manager does not support this, I mus find a different way.

BR

Kasper

0 Kudos
Reply
1 Reply

1,495 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is this intentional?
-- No, I guess it's still related to the software configuration.
2) Am I the only one with this requirement?
-- Yes, it seems like that.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply