Secure Firmware Update on a Mass Production Board Using RT1064

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Secure Firmware Update on a Mass Production Board Using RT1064

2,147 次查看
kbsidi
Contributor II

We have developed a mass production board using the RT1064.


The Boot Mode Switch is fixed to 0x0010.


We would like to implement firmware updates with the Secure feature applied.


Could you please let us know if this is possible, and if so, how it can be achieved?

标签 (1)
0 项奖励
回复
3 回复数

2,126 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @kbsidi ,

Thanks for your interest in NXP MIMXRT series!

Your application scenario is feasible and you are advised to refer to the OTA related project in the SDK. It uses imgtool to sign the image and then performs an OTA upgrade over the network. Also, SBL and SFW are good reference projects and you can find them on github. https://www.nxp.com/docs/en/user-guide/MCUOTASBLSFWUG.pdf

Best,
Gavin

2,115 次查看
kbsidi
Contributor II
My custom board does not have wireless communication capabilities.
I would like to know if it is possible to implement this using a USB-based method.
Thank you.
Alex.
0 项奖励
回复

2,100 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Yes, using USB is also possible. You can check out the usb_dfu project.