SRAM_DTC read/Write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRAM_DTC read/Write

1,272 Views
vijayc1
Contributor II

Hai i am using IMXRT1062 board i need to access the Internal SRAM_DTC to read and write can anyone help me to sort this ?

0 Kudos
Reply
1 Reply

1,257 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

If you need to save something in specific sections of RAM you can refer to: Relocating Code and Data Using the MCUXpresso IDE - NXP Community

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 Kudos
Reply