Running TensorFlow Lite on HiFi-Mini DSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Running TensorFlow Lite on HiFi-Mini DSP

4,068 次查看
dele_ogunjumelo
Contributor I

Please, has any one been able to run a TensorFlow Lite For Micro based application on a HiFi Mini DSP? I am using the NXP i.MX RT600 board.

标签 (1)
0 项奖励
回复
4 回复数

3,959 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Dele Ogunjumelo,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I've created an eIQ demo which uses the TensorFlow Lite library, however, it runs the Cortex-M33 core, next, I will try to run this demo by another core: HiFi4 DSP.
In further, I was wondering if you can share what progress you get and the encountered issue now.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,959 次查看
dele_ogunjumelo
Contributor I

Hi jeremyzhou‌,

With regards to getting the Hello world TFLM application to run on the HiFi DSP, I have followed the steps in TensorFlow Repo to build TFLM for Cadence Tensilica HiFi DSPs.  I have also got the sample DSP applications (DSP MU polling) to run on the RT600 board. I am currently working on integrating the HiFi NN libraries into the sample HelloWorld application, and also working on configuring the DSP using similar steps as seen in the sample apps.

0 项奖励
回复

3,959 次查看
jeremyzhou
NXP Employee
NXP Employee

HiDele Ogunjumelo,

I'm glad to hear that, I was wondering if you can upload the demos to community and share the steps of implementing, I think it's very useful for other engineers.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

3,959 次查看
dele_ogunjumelo
Contributor I

Hi jeremyzhou‌,

I have not got a working Demo , I would upload one when i get a working demo.  For steps on building TFLM for Cadence Tensilica HiFi DSPs, please see link below: -

tensorflow/README.md at be2c7869f592c0fbfae31e1cd1c9bae317f58695 · tensorflow/tensorflow · GitHub 

Regards,

Dele

0 项奖励
回复