RT500 OTP Fuse Map and programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT500 OTP Fuse Map and programming

1,585件の閲覧回数
GR-Grinn
Contributor II

Hi!

We're trying to prepare a way to set up RT555 booting in OTP.

  1. Are there any updates related to RT500 OTP Fuse Map availability since this question was askedRT500 OTP Fuse Map ?
  2. It is possible to program OTP using debug probe directly (MCU-Link or JLink) or communication with the bootloader is necessary?

We're trying to find a way to work around design fault in our current PCB design, with sets ISP pins in Serial Download mode, rather than FLEXSPI Boot. We would prefer solution that does not require hardware modifications, as UART pins used in the Serial Download mode are not easily accessible.

With regards

タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,525件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Hi @GR-Grinn 

Thank you for your interest in NXP Semiconductor products.


1. Are there any updates related to RT500 OTP Fuse Map availability since this question was askedRT500 OTP Fuse Map ?

--> Thanks for your reminder. After checking, the OTP map is still missing in RT5xx RM, I have asked document team for an update.

 

2. It is possible to program OTP using debug probe directly (MCU-Link or JLink) or communication with the bootloader is necessary?

--  It is possbile to develop an application using 18.7.4 OTP Driver APIs mentioned in RM.

Please note: Use debug probe to download and execute the firmware for OTP provisioning, JLINK commander cannot support OTP writing.

 

B.R,

Sam

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,163件の閲覧回数
GR-Grinn
Contributor II

Is there any progress regarding OTP Fuse Map for RT500?

タグ(2)
0 件の賞賛
返信