RT1176 with camera interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 with camera interface

1,657 Views
selvamras
Contributor I
  • Hi
  •    I need to interface two independent camera with RT1176 PROCESSOR through MiPi-CSI  interface. But this processor has only one MiPi-csi interfece. Please tell me how do we connect. Can i use a MiPi mux to connect two camera with single MiPi-CSI interface of RT1176?
0 Kudos
Reply
1 Reply

1,650 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @selvamras 

 Please check this picture at first, you will be more clear:

kerryzhou_0-1624608591683.png

You can find parallels CSI and the Mipi-CSI will connect to the CSI at last, you can connect two CSI modues, one to parallels CSI, one to MIPI-CSI. But these two CSI can't work at the same time. So, normally, we can use one as the MIPI-CSI, another one, we can use the flexIO to simulate the CSI, this method, you can use two cameras at the same time, about the flexIO csi, we have an application note:

AN12686

https://www.nxp.com/docs/en/application-note/AN12686.pdf

https://www.nxp.com/docs/en/application-note-software/AN12686SW.zip

 

Wish it helps you!

Best Regards,

kerry

 

 

0 Kudos
Reply