RT1176 USB Not Working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1176 USB Not Working

1,523 次查看
Tariq_Al
Contributor II

Hello, 

I designed a custom board based on MIMXRT1176CVM8A and connected the USB1 to a micro USB connector, but the PC does not identify the board using the MXUxpresso Secure Provisioning. What are the reasons for this? 

Regarding the circuits, 

Tariq_Al_0-1745146040305.png

 

For the micro-USB connector: 

Tariq_Al_1-1745146107899.png

 

 

 

0 项奖励
回复
3 回复数

1,485 次查看
Tariq_Al
Contributor II

Thank you for your reply. 

1. My board powered correctly, and I can work around the MCU, reading from RAM and flashing the QSPI. 

2. I am sure to choose the boot in serial mode before I power up the board, but even after booting, the USB doesn't work. 

3. For the HW design USB, I already took the circuit, connections, and components from the EVK design. 

0 项奖励
回复

1,443 次查看
mayliu1
NXP Employee
NXP Employee

Hi @Tariq_Al ,

 

Thanks for your updated information.

Please check whether the USB connection is normal and replace the cable; 

Please use a multimeter to test whether the USB power supply is normal ; Please check the status of the USB ID signal.

mayliu1_0-1745293835041.png

I suggest you can compare your custom board with the MIMXRT1170-EVKB development board status to see if there are any differences.

  

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

0 项奖励
回复

1,498 次查看
mayliu1
NXP Employee
NXP Employee

Hi @Tariq_Al ,

 

Thank you so much for your interest in our products and for using our community.

Regarding your question, I suggest you check the following points:

1. Verify whether your custom board powers on successfully.

For example, the next Fig shows the power control logic of the IMXRT1170 EVK board.

mayliu1_2-1745207534569.png

 

2. Before using the MXUxpresso Secure Provisioning, have you set the BOOT_MODE to "Serial Downloader"?

 

mayliu1_1-1745207101007.png

3:  As for your USB HW design, I suggest you can refer to MIMXRT1170-EVK  board design.

MIMXRT1170-EVK | NXP Semiconductors

mayliu1_3-1745207649574.png

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu