RT1176 EVK running failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 EVK running failed

885 Views
macro_lee
Contributor I

mdk keil (RT1176 EVK):

when i select the flexspi_nor_sdram release project,after i rebuild it and load to the rt1176,evk board can not run well (just like dead crash),the same with putting the reset button;

when i select the flexspi_nor_sdram debug project,after i rebuild it and load to the rt1176,evk board can run well(debug run and then stoped the debug window),but when i putting the reset button;the evk board crashed;

i try to using the secure provising tool to connect the evk board but always failed(through the sdp usb port, tip: boot mode (both 00 and 01 all used to try))

that‘s why, thanks for your help

Best Regards!

0 Kudos
Reply
1 Reply

828 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you are doing all ok the is probably that you have a damage board, please contact your vendor for this reason.

Regards

0 Kudos
Reply