RT1172 with external SDRAM via SEMC interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1172 with external SDRAM via SEMC interface

Jump to solution
813 Views
AndreiZi
Contributor I

Hello,

 

I have an external SDRAM (AS4C16M16SA from Alliance datasheet is attached) connected to SEMC interface of MCU.

I use the SDK example semc_cm7.

The configurations are set in function SDRAM_InitSEMC();

As far as I understand here the parameters:

static status_t SDRAM_InitSEMC(void)

{

semc_config_t config;

semc_sdram_config_t sdramconfig;

uint32_t clockFrq = EXAMPLE_SEMC_CLK_FREQ;

 

/* Initializes the MAC configure structure to zero. */

memset(&config, 0, sizeof(semc_config_t));

memset(&sdramconfig, 0, sizeof(semc_sdram_config_t));

 

/* Initialize SEMC. */

SEMC_GetDefaultConfig(&config);

config.dqsMode = kSEMC_Loopbackinternal; /* For more accurate timing. */

SEMC_Init(SEMC, &config);

 

/* Configure SDRAM. */

sdramconfig.csxPinMux = kSEMC_MUXCSX0; // TODO understand what is this ???

sdramconfig.address = EXAMPLE_SEMC_START_ADDRESS;

sdramconfig.memsize_kbytes = 32 * 1024; /* 32 MByte = 4 M Words * 16 Bit * 4 Banks */

sdramconfig.portSize = kSEMC_PortSize16Bit; /* one 16-bit SDRAM port size*/

sdramconfig.burstLen = kSEMC_Sdram_BurstLen8;

sdramconfig.columnAddrBitNum = kSEMC_SdramColunm_9bit; // TODO

sdramconfig.casLatency = kSEMC_LatencyThree; // 2-3 TODO

sdramconfig.tPrecharge2Act_Ns = 21; /* tRP 18ns - 21ns : Pre-charge to refresh/row activate command (same bank) */

sdramconfig.tAct2ReadWrite_Ns = 21; /* tRCD 18ns - 21ns : RAS# to CAS# delay (same bank) */

sdramconfig.tRefreshRecovery_Ns = 70; /* Use the maximum of the (tRFC , tXSR). */

sdramconfig.tWriteRecovery_Ns = 14; /* tWR 12ns - 14ns : Write recovery time */

sdramconfig.tCkeOff_Ns = 42; /* The minimum cycle of SDRAM CLK off state. CKE is off in self refresh at a minimum period tRAS.*/

sdramconfig.tAct2Prechage_Ns = 42; /* tRAS 42ns */

sdramconfig.tSelfRefRecovery_Ns = 70; // TODO from here down all the lines

sdramconfig.tRefresh2Refresh_Ns = 60;

sdramconfig.tAct2Act_Ns = 10; /* tRC/tRDD 10ns */

sdramconfig.tPrescalePeriod_Ns = 160 * (1000000000 / clockFrq);

sdramconfig.refreshPeriod_nsPerRow = 64 * 1000000 / 8192; /* 64ms/8192 */

sdramconfig.refreshUrgThreshold = sdramconfig.refreshPeriod_nsPerRow;

sdramconfig.refreshBurstLen = 1;

sdramconfig.delayChain = 6; /* For all temperatures. */

sdramconfig.autofreshTimes = 8; /* An additional eight Auto Refresh cycles (CBR) are also required before or after

programming the Mode Register to ensure proper subsequent operation. */

 

return SEMC_ConfigureSDRAM(SEMC, kSEMC_SDRAM_CS0, &sdramconfig, clockFrq);

}

 

As I am a new in SDRAM I'll appreciate for some brief explanations on all the fields.

 

Few things are unclear:

1. sdramconfig.portSize - how I decide which one is to set?

2. sdramconfig.burstLen - what are consideration to choose one? pluses and minuses?

3. sdramconfig.casLatency - the same question

4. sdramconfig.refreshPeriod_nsPerRow - how to define?

5. sdramconfig.tPrescalePeriod_Ns - how to calculate?

 

How do I set the SDRAM clock frequency? In SDK example it comes from CLOCK_GetRootClockFreq(kCLOCK_Root_Semc);

How I set it for my custom SDRAM?

 

In

Appreciate your support.

Andrei

0 Kudos
Reply
1 Solution
679 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

SEMC clock can be ajdusted with config tools so it matches your devices speed. 

SEMC access address with this scheme:

Omar_Anguiano_0-1726533461267.png

Best regards,
Omar

 

View solution in original post

0 Kudos
Reply
13 Replies
733 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello.
I will help you clarify how to chose the right parameter for you device, some of these parameters depend on the SDRAM datasheet while other there are some calculations to make.

1.Portsize, it refers to the data bus size of the memory. Your device is 16bit but you can use two SDRAM for 32bit port size(refer to the EVK).

2. The higher the burst higher performance as more data is transferred however it is needed to consider the refresh commands.

3. It depends on the device, higher performance when latency is low. The value will depend on your programed CAS latency of your memory.

4 and 5. Please refer to his example:

Omar_Anguiano_0-1726002705073.png

 

Best regards,
Omar

0 Kudos
Reply
468 Views
Littell
Contributor II

What document is this example taken from?  It implies there's a step-by-step initialization example that can be used as a template to identify the calculations needed to support a particular SDRAM device and create a correct DCD.

0 Kudos
Reply
274 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Littell 

We apologize for the delayed response, my colleague is currently out of the office, and I want to keep the follow up. 


I do not have the material related to the example he is showing, as it might be material that it is not officially released/stored on nxp.com, for example custom hands-on trainings to customers.


Could you help me to create another thread to keep a cleaner follow up? Per my understanding , you need step by step guide to enable SDRAM, ( calculations and DCD) during boot time. It is possible that you share with us the SDRAM part number that you want to use? Along its features? In the new thread. We may not have additional information on this, but we can adapt to your use case scenario, or have already something for your SDRAM model.

We appreciate your interest in our products, thank you.

Diego

0 Kudos
Reply
255 Views
AndreiZi
Contributor I

Hi Diego,

I also have a difficulties to make a proper DCD and/or use it correctly. My device is based on NAND flash memory connected by FlexSPI1 and external SDRAM (AS4C16M16SA-7BCN) connected by SEMC interface. Although I am able to configure it properly during the code and make it work properly I cannot configure it run as a main RAM in system and use during the boot to copy image from flash to external SDRAM and run from it.  

Hope you can give me a hand with this issue too.

Kind regards,

Andrei

0 Kudos
Reply
155 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @AndreiZi 

I am sorry for the delayed response, I manually subscribed to the ticket to get updates, but I did not catch them.

Have you tried quiclkly testing the SEMC SDRAM XMCD using our Secure Provisioning Tool? There are 3 paramters that we can edit. 

diego_charles_0-1731517950751.png

Thank you for your patience. 

Diego

 

 

 

 

0 Kudos
Reply
136 Views
AndreiZi
Contributor I

Hi Diego,

Thank you for your response. Actually I already figured out this option and it works with some limitation of size. I cannot even build application with size more than ~1Mbytes. See attached print screen.

So it worked with code:

BOARD_SDRAM:      860864 B     32704 KB      2.57%

BOARD_SDRAM:     1052864 B     32704 KB      3.14%

 

And stopped to work with code size:

BOARD_SDRAM:     1628840 B     32704 KB      4.86%

BOARD_SDRAM:     1244864 B     32704 KB      3.72%

BOARD_SDRAM:     1148864 B     32704 KB      3.43%

 

The error message I see it before I am able to press button Build Image:

 

ERROR: Image size 0x001147B8 is greater than region available for the following image copies:

- image copy #0 starting at block index 2, size 0x00100000

Status of the operation: Failure: Operation `Build image` failed with an error: There are problems in settings, see Log for details.

 

Seems it somehow connected to the 0x100000 code size.

Please advise me with this issue.

 

Thank you in advance.

 

Kind regards,

Andrei Zinenko

0 Kudos
Reply
21 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello!

It seems that the error is set as the linker thinks that the image from NAND will be copied to internal RAM. Please rearenge the linker so the image is set to be copied directly to SDRAM. 

Solved: NAND FLASH XIP and boot modes - NXP Community

Best regards,
Omar

0 Kudos
Reply
315 Views
Littell
Contributor II

Hello?

0 Kudos
Reply
812 Views
AndreiZi
Contributor I

1.  It always write to defined address + size of 1 data offset. I.e. If I try to write to address
#define EXAMPLE_SEMC_START_ADDRESS (0x80000000U)
It will write to (I see it in debugger memory window and later in read buffer) 0x80000002U address in case of data size of uint16_t.
2. Each 16th write access fails, and I see as a result or Zero or some garbage, see attached read buffer signed with red

0 Kudos
Reply
703 Views
AndreiZi
Contributor I

Thank you for your response. Unfortunately, I am in vacation until end of September. I will check your suggest when I come back.

I did not see how to configure the SDRAM clock speed. My memory is 143MHz if I remember correctly. SO original example from SDK is too fast? 

And why it writes data in memory with offset of 2 bytes?

 

Kind regards,

Andrei

0 Kudos
Reply
680 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

SEMC clock can be ajdusted with config tools so it matches your devices speed. 

SEMC access address with this scheme:

Omar_Anguiano_0-1726533461267.png

Best regards,
Omar

 

0 Kudos
Reply
541 Views
AndreiZi
Contributor I
Thank you for your help
0 Kudos
Reply
810 Views
AndreiZi
Contributor I
 
0 Kudos
Reply