The ADC on the RT1170 series processor is documented to have 3 selectable reference voltages. Those are 1.8V, 3.3V and an external V_REFH. A reference source can be selected via the REFSEL field in the CFG register of the ADC.
What I'm unable to find is which setting in this field corresponds to which reference voltage. The options for this field are documented as "See the chip configuration information on the voltage reference options specific to this packaged device.", but I can't find this information anywhere?
Which source is selected when setting the filed to 0b00, which when setting it to 0b01 and which when setting it to 0b10?
Thank you Carlos for that answer. Is there an error associated with using the 30/64 scaling option? How is it implemented inside of the RT1170?
Edit: I thought the question I asked was related and short enough to add to this thread, but I've decided I have more questions that are related and it would be best to open a new one. Here is another thread on this topic that is worth reading: