RT1061 does not boot when code size on flash memory is exceed 256k

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1061 does not boot when code size on flash memory is exceed 256k

1,073 Views
Mithy
Contributor I

Hi, I am using MIMXRT1061DVL6B with 8MB flash memory from winbond.

the problem is once the code size on flash is exceed 256kbyte.

RT1061 is not properly booted.

is there any possible reason and solution for it?

I am using this device for consumer electronics.

thank you

0 Kudos
Reply
1 Reply

1,053 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I reviewed your information and I have these questions.

Are you using the EVK? If yes, the boot mode should be at internal boot.
How do you determine what is not going well? Could you share the LOG?

What is the number of the memory?

Best regards,
Pavel

0 Kudos
Reply