RT1060 implementing code protection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1060 implementing code protection

2,171件の閲覧回数
e_v_spronsen
Contributor III

Hi,

Is there any documentation on how to setup code protection and to get basic understanding how it works?

Thanks,

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,105件の閲覧回数
mjbcswitzerland
Specialist V

Hi Ernst

These are the documents that are readily accessible:
- https://community.nxp.com/docs/DOC-344919
- https://www.nxp.com/docs/en/application-note/AN12419.pdf
- https://www.nxp.com/docs/en/application-note/AN12800.pdf

Generally check out the 1060 documents and application notes at
https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-...

but some security related ones may only be available via your FAE.

For a simpler to use method that increases security with AES256 encryption and integrates code and clone protection together with boot loading and OTA update concept you can also use the uTasker project:
https://www.utasker.com/docs/iMX/Loader.pdf
https://www.youtube.com/watch?v=2XfgZq19XDw&list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&index=3
which works compatibly on i.MX RT 1010 to i.MX RT 1064

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

0 件の賞賛
返信

2,105件の閲覧回数
e_v_spronsen
Contributor III

Mark,

Thanks for the retailed reply. We already have our own ecosystem so i really like to integrate secure boot into it. 

I try to find a NXP FAE for some more info and hopefully some examples.

Thanks.

0 件の賞賛
返信