RT105x FlexRAM configuration using the DCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT105x FlexRAM configuration using the DCD

2,065件の閲覧回数
gaetano81
Contributor I

Hello Yuri,

is it possible to set  IOMUXC_GPR_GPR17 and IOMUXC_GPR_GPR16 using Device Configuration Data?

 

Regards 

Gaetano

ラベル(1)
0 件の賞賛
返信
1 返信

1,848件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   i.MX RT1050 Reference Manual (Rev. 1, 03/2018) mentions the list of allowable
blocks and target addresses for the chip, which may be written, using the DCD,

but the list is skipped. Generally IOMUX_GPR area should be included in the valid

DCD ranges; in any case customers  can also use a plugin image running in OCRAM.  


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信