RT1050 connect with two camera

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1050 connect with two camera

2,278 次查看
captain_huang
Contributor I

In the i.MX RT1050 Processor Reference Manual  :

pastedImage_2.png

it said the rt1050 support to connect with two camera sensors. so anybody who can tell me hao to use this function. i need to connect with two camera in my application.

tks!

标签 (1)
0 项奖励
回复
1 回复

2,140 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chao

one can look at AN12103 and its software example to modify sources

for receiving data from two cameras

AN12103 Developing a simple UVC device based on i.MX RT1050

https://www.nxp.com/docs/en/application-note/AN12103.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复