When using the touch screen controller (TSC) on the RT1050 - in 4 pin mode - do you have to leave pin GPIO_AD_B1_11 as a no connect, or can it be used for other functionality?
I also couldn't find any demos using this module in the RT1050's SDK, are there any?
Thanks!
已解决! 转到解答。
Hello,
>>do you have to leave pin GPIO_AD_B1_11 as a no connect, or can it be used for other functionality?
Yes. The pin can be used to other function.
>>I also couldn't find any demos using this module in the RT1050's SDK, are there any?
Unfortunately, There is not any demo for it. Only refer to the driver fsl_tsc.h/fsl_tsc.c in SDK_2.5.0_EVK-MIMXRT1050\devices\MIMXRT1050\drivers.
Hello,
>>do you have to leave pin GPIO_AD_B1_11 as a no connect, or can it be used for other functionality?
Yes. The pin can be used to other function.
>>I also couldn't find any demos using this module in the RT1050's SDK, are there any?
Unfortunately, There is not any demo for it. Only refer to the driver fsl_tsc.h/fsl_tsc.c in SDK_2.5.0_EVK-MIMXRT1050\devices\MIMXRT1050\drivers.
One follow-up question fangfang
Is it possible to use different ADC pins for the TSC.
We're using GPIO_AD_B1_12 - GPIO_AD_B1_15 for the CSI interface, and we're using the JTAG pins - so we can't remove CSI_DATA_02 - CSI_DATA_05 from the pins that the RM says are the only TSC pins.
Is it not possible to use TSC on other pins, like:
GPIO_AD_B1_08, GPIO_AD_B1_07, GPIO_AD_B1_06, GPIO_AD_B1_05?