RT1050 PWM resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 PWM resolution

1,350件の閲覧回数
hitwangweiqi
Contributor I

Hi team,

I am a beginner for RT1050.

For KV5x PWM module, it is noted in datasheet what is the highest PWM resolution (eg.260ns). However, I did not notice the similar discription in RT1050, what is the data for this device?

Besides, can we support highest resolution for period, phase and deadband? Or we can just realize part of that?

Regards,

Bruno

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,242件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Bruno Wang,

There's the reply from the AE team.

On the RT10xx products, the eFlexPWMs get their clock from ipg_clk_root. The max frequency for ipg_clk_root is 150MHz, so the resolution without even using any of the fractional options can already hit 6.67ns.

Hope this helps,

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,242件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Bruno Wang,

Whether you can share your company name and Website, AE team need to register this information.


Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,242件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Bruno Wang

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
It seems that the datasheet misses the specification about PWM resolution, I'll contact with the AE team for checking and inform you later.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信