TL;DR - We can't seem to download and debug an RT1050 program image to a board that has a QSPI flash attached to the secondary FlexSPI pinmux location.
We've constructed a custom board based on the RT1050 (MIMXRT1052CVJ5B). Because of how many serial I/O ports we had to allocate, we did not use an octal HyperFlash like that on the EVKB; rather, we connected a QSPI flash (S25FL256L) to the secondary pinmux location, as so:
QSPI | FLEXSPI | GPIO | Ball |
---|---|---|---|
CS* | FLEXSPI_A_SS0_B | GPIO_B1_15 | J14 |
SCLK | FLEXSPI_A_SCLK | GPIO_B1_14 | G12 |
D3 | FLEXSPI_A_DATA3 | GPIO_B1_10 | L13 |
D2 | FLEXSPI_A_DATA2 | GPIO_B1_11 | J13 |
D1 | FLEXSPI_A_DATA1 | GPIO_B1_12 | H12 |
D0 | FLEXSPI_A_DATA0 | GPIO_B1_13 | H11 |
We also replicated the configuration DIP switches that are present on the EVKB. Referring to Table 8-9 of the RT1050 manual, I could see that BOOT_CFG2[2:0] (i.e. BOOT_CFG[10:8]) needed to be "111" for "QSPI device supports 3B read by default (on secondary pinmux option)", not "010" for "HyperFlash 1.8V". So I set the DIP switches to "0000 0011 0110" to select Flash Type 111 and Boot Type 10 (internal boot). And it appears that I've set the DIP switches correctly, because if I reset the processor, I see this on the QSPI pins:
My Logic pod isn't fast enough to capture the actual data that's being transmitted (nor can it decode QSPI), but I can see three bursts... the first two are about 3.7 us each, and the big one is about 259 us long.
The debug pod (SEGGER J-Link Pro) connects OK with the CPU; there was some initial confusion over what debug mode to use, but we now have SWD selected. When I try to program and download an image, the SEGGER four-bar programming window appears, it gets to 25% compare a touch slowly, then 50%, then the window disappears:
Then the debugger lands at address 0x20b4f2 (the actual address for any given run is somewhat random, I got 0x20d136 another time):
And you pretty much can't do anything at this point. The addresses clearly reside inside the ROM region, so presumably the RT1050 was not able to boot successfully and remained in its ROM program.
Here's what I see on my Logic probe while launching the debug session:
That big burst in the middle there is a whole bunch of transfers, each lasting about 259 us and spaced apart every 6-7 ms. So, any ideas what we're doing wrong? I certainly can't rule out a hardware issue, but it looks like the signals between the CPU and the QSPI flash are OK. Maybe one has to do some additional configuration of the J-Link debug launch. Where should I start?
已解决! 转到解答。
David,
Sorry if I confused matters, was trying to help. I went through a _lot_ of pain getting this configuration running, so I'd like to help a fellow sufferer
JLink certainly can program a blank flash on the secondary pinmux, that is (now!) what I do all of the time. I'm on 1021, but I can't imagine there are differences. Given that your CPU is trying to access the flash I would be inclined to suspect you've got the various initialisation tables a bit wrong (or, more probably, MCUX has, since I don't think you generate them manually in a MCUX configuration).
I'm running NuttX and the start of my flash looks like this;
60000000 A __boot_hdr_start__ 60000000 R flash_config 60001000 A __boot_hdr_conf__ 60001000 R g_image_vector_table 60001020 R g_boot_data 60001030 A __boot_hdr_end__ 60002000 A _stext 60002000 T _vectors
...and the various data in each of those tables is as follows;
000000 4346 4246 0400 5601 0000 0000 0300 0003 000010 0001 0000 0401 0000 0040 0000 0000 0000 000020 0000 0000 0000 0000 0000 0000 0000 0000 <SNIP> 001000 00d1 4120 2000 6000 0000 0000 0000 0000 001010 1020 6000 1000 6000 0000 0000 0000 0000 001020 0000 6000 ffff 1f7f 0000 0000 ffff ffff 001030 ffff ffff ffff ffff ffff ffff ffff ffff
The source that I build those tables from is;
__attribute__((section(".boot_hdr.conf"))) const struct flexspi_nor_config_s flash_config = { .mem_config = { .tag = FLEXSPI_CFG_BLK_TAG, .version = FLEXSPI_CFG_BLK_VERSION, .read_sample_clksrc = FLASH_READ_SAMPLE_CLK_LOOPBACK_INTERNELLY, .cs_hold_time = 3u, .cs_setup_time = 3u, .device_mode_cfg_enable = true, .device_mode_seq.seq_num= 1, .device_mode_seq.seq_id = 4, /* These commands set the Quad bit */ .device_mode_arg = 0x40, /* on the flash to drive 4 pins. */ .device_type = FLEXSPI_DEVICE_TYPE_SERIAL_NOR, .sflash_pad_type = SERIAL_FLASH_4PADS, .serial_clk_freq = FLEXSPI_SERIAL_CLKFREQ_100MHz, .sflash_a1size = 8u * 1024u * 1024u, .data_valid_time = {16u, 16u}, /* .controller_misc_option = (1 << FLEXSPIMISC_OFFSET_PAD_SETTING_OVERRIDE_EN), */ /* .cspad_setting_override = 1|(1<<3)|(3<<6), */ /* .sclkpad_setting_override = (7<<3)|(3<<6), */ /* .datapad_setting_override = (2<<3)|(3<<6), */ /* .dqspad_setting_override = 0, */ .lookup_table = { /* 0 - Quad Input/output read sequence - with optimised XIP support */ [0]=FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18), [1]=FLEXSPI_LUT_SEQ(MODE8_SDR, FLEXSPI_4PAD, 0xA0, DUMMY_SDR, FLEXSPI_4PAD, 0x04), [2]=FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_4PAD, 0x04, JMP_ON_CS, 0, 1), /* 1 - Read Status */ [1*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x01), /* 3 - Write Enable */ [3*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP, 0, 0), /* 4 - Write status */ [4*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x01, WRITE_SDR, FLEXSPI_1PAD, 0x1), /* 5 - Erase Sector */ [5*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD7, RADDR_SDR, FLEXSPI_1PAD, 0x18), /* 9 - Page Program */ [9*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x02, RADDR_SDR, FLEXSPI_1PAD, 0x18), [9*4+1] = FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x8, STOP, FLEXSPI_1PAD, 0x0), /* 11 - Chip Erase */ [11*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xC7, STOP, FLEXSPI_1PAD, 0x0), }, }, .page_size = 256u, .sector_size = 4u * 1024u, .blocksize = 32u * 1024u, .is_uniform_blocksize = false, };__attribute__((section(".boot_hdr.ivt"))) const struct ivt_s g_image_vector_table = { IVT_HEADER, /* IVT Header */ 0x60002000, /* Image Entry Function */ IVT_RSVD, /* Reserved = 0 */ (uint32_t)DCD_ADDRESS, /* Address where DCD information is stored */ (uint32_t)BOOT_DATA_ADDRESS, /* Address where BOOT Data Structure is stored */ (uint32_t)&g_image_vector_table, /* Pointer to IVT Self (absolute address) */ (uint32_t)CSF_ADDRESS, /* Address where CSF file is stored */ IVT_RSVD /* Reserved = 0 */ }; __attribute__((section(".boot_hdr.boot_data"))) const struct boot_data_s g_boot_data = { FLASH_BASE, /* boot start location */ (FLASH_END - FLASH_BASE), /* size */ PLUGIN_FLAG, /* Plugin flag*/ 0xFFFFFFFF /* empty - extra data word */ };
Drop me a note if you want an image to just try burning into the chip to see if it will boot from it...you should be able to do that from JLinkExe which would at least put to bed any concern over hardware issues.
Regards
DAVE
Hi kerryzhou,
Well, good news and bad news. Bad news, I've given up on making this Cypress S25FL256S flash work. I'm simply not equipped or prepared to go into an exhaustive analysis of what's wrong with my present setup.
Good news, we got a couple of ISSI IS25LP064A chips in, I replaced the Cypress with the ISSI on one of our prototypes, built my app (with a properly modified DCD header), dialed up the correct settings in the MCU Config Tool, and the tool programmed the board successfully. I then hacked my SEGGER XML file (still annoyed that's a step), downloaded via the debugger, and whaddaya know, the damn thing actually works. For reference, here is how I modified evkbimxrt1050_flexspi_nor_config.c (following exactly what dmarples laid out):
/* Width of flash addresses (either 24 or 32). */
#define QSPI_ADDR_WIDTH 24u
#ifdef USE_QSPI
const flexspi_nor_config_t qspi_config = {
.memConfig = {
.tag = FLEXSPI_CFG_BLK_TAG,
.version = FLEXSPI_CFG_BLK_VERSION,
.readSampleClkSrc = kFlexSPIReadSampleClk_LoopbackInternally,
.csHoldTime = 3u,
.csSetupTime = 3u,
/* This defines the sequence to use to set the QUAD bit.
* Command 0x01 writes the status register and sets bit 6 (0x40).
* SR = 0x40 (bit 6 = QE Quad Enable, all other bits to 0) */
.deviceModeCfgEnable = true,
.deviceModeSeq.seqNum = 1,
.deviceModeSeq.seqId = 4,
.deviceModeArg = 0x40,
/* Device geometry, I/O, and speed. */
.deviceType = kFlexSpiDeviceType_SerialNOR,
.sflashPadType = kSerialFlash_4Pads,
.serialClkFreq = kFlexSpiSerialClk_100MHz,
.sflashA1Size = 8u * 1024u * 1024u,
.dataValidTime = {16u, 16u},
/* Lookup table for flash commands for this device. Up to 8 instructions
* can be defined for each LUT table location. Each instruction is 16 bits,
* and the data structure organizes them as 32-bit words (for some reason). */
.lookupTable = {
/* 0 - Quad Input/output read sequence - with optimized XIP support */
[0*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB,
RADDR_SDR, FLEXSPI_4PAD, QSPI_ADDR_WIDTH),
[0*4+1] = FLEXSPI_LUT_SEQ(MODE8_SDR, FLEXSPI_4PAD, 0xA0, // 2 dummy cycles
DUMMY_SDR, FLEXSPI_4PAD, 4), // 4 dummy cycles
[0*4+2] = FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_4PAD, 4,
JMP_ON_CS, FLEXSPI_1PAD, 1),
/* 1 - Read Status */
[1*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05,
READ_SDR, FLEXSPI_1PAD, 1), // Read 1 byte
/* 3 - Write Enable */
[3*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06,
STOP, FLEXSPI_1PAD, 0),
/* 4 - Write status */
[4*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x01,
WRITE_SDR, FLEXSPI_1PAD, 1), // Write 1 byte
/* 5 - Erase Sector */
[5*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD7, // Sector Erase, 1-bit
RADDR_SDR, FLEXSPI_1PAD, QSPI_ADDR_WIDTH),
/* 9 - Page Program */
[9*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x02,
RADDR_SDR, FLEXSPI_1PAD, QSPI_ADDR_WIDTH),
[9*4+1] = FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x08, // any non-zero value
STOP, FLEXSPI_1PAD, 0),
/* 11 - Chip Erase */
[11*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xC7,
STOP, FLEXSPI_1PAD, 0x0),
},
},
.pageSize = 256u,
.sectorSize = 4u * 1024u,
.blockSize = 32u * 1024u,
.isUniformBlockSize = false,
};
#else
const flexspi_nor_config_t hyperflash_config = {
[...]
};
#endif
It also turns out that because of some changes to the system over the past couple of months, it will be possible in Rev. B of our board to shuffle some things around and get an 8-bit HyperFlash connected to the primary pinmux location, so we won't have any of these issues to deal with in the future. So at least we proved that yes, we can boot off the secondary pinmux location, even if we weren't able to do it with the QSPI flash we originally selected. Thanks everyone for all the assistance.
I had been using the flash config structure referenced inthis thread on the evaluation board, and was able to debug using the JLink after modifying the JLinkDevices.xml file.
Our custom boards that use the IS25WP064A Quad SPI Flash arrived recently, and I had been having no luck getting debugging with the JLink working with them. After double checking the BOOT_MODE/BOOT_CONFIG settings several times, I changed my flash config structure to this one, and JLink debugging started working immediately. I'm not sure what difference exists between the boards (they were designed to mimic the evaluation board Quad SPI flash layout) or which setting "made it work," but I'm glad this fixed it.
Thanks for the help!
David,
Sorry if I confused matters, was trying to help. I went through a _lot_ of pain getting this configuration running, so I'd like to help a fellow sufferer
JLink certainly can program a blank flash on the secondary pinmux, that is (now!) what I do all of the time. I'm on 1021, but I can't imagine there are differences. Given that your CPU is trying to access the flash I would be inclined to suspect you've got the various initialisation tables a bit wrong (or, more probably, MCUX has, since I don't think you generate them manually in a MCUX configuration).
I'm running NuttX and the start of my flash looks like this;
60000000 A __boot_hdr_start__ 60000000 R flash_config 60001000 A __boot_hdr_conf__ 60001000 R g_image_vector_table 60001020 R g_boot_data 60001030 A __boot_hdr_end__ 60002000 A _stext 60002000 T _vectors
...and the various data in each of those tables is as follows;
000000 4346 4246 0400 5601 0000 0000 0300 0003 000010 0001 0000 0401 0000 0040 0000 0000 0000 000020 0000 0000 0000 0000 0000 0000 0000 0000 <SNIP> 001000 00d1 4120 2000 6000 0000 0000 0000 0000 001010 1020 6000 1000 6000 0000 0000 0000 0000 001020 0000 6000 ffff 1f7f 0000 0000 ffff ffff 001030 ffff ffff ffff ffff ffff ffff ffff ffff
The source that I build those tables from is;
__attribute__((section(".boot_hdr.conf"))) const struct flexspi_nor_config_s flash_config = { .mem_config = { .tag = FLEXSPI_CFG_BLK_TAG, .version = FLEXSPI_CFG_BLK_VERSION, .read_sample_clksrc = FLASH_READ_SAMPLE_CLK_LOOPBACK_INTERNELLY, .cs_hold_time = 3u, .cs_setup_time = 3u, .device_mode_cfg_enable = true, .device_mode_seq.seq_num= 1, .device_mode_seq.seq_id = 4, /* These commands set the Quad bit */ .device_mode_arg = 0x40, /* on the flash to drive 4 pins. */ .device_type = FLEXSPI_DEVICE_TYPE_SERIAL_NOR, .sflash_pad_type = SERIAL_FLASH_4PADS, .serial_clk_freq = FLEXSPI_SERIAL_CLKFREQ_100MHz, .sflash_a1size = 8u * 1024u * 1024u, .data_valid_time = {16u, 16u}, /* .controller_misc_option = (1 << FLEXSPIMISC_OFFSET_PAD_SETTING_OVERRIDE_EN), */ /* .cspad_setting_override = 1|(1<<3)|(3<<6), */ /* .sclkpad_setting_override = (7<<3)|(3<<6), */ /* .datapad_setting_override = (2<<3)|(3<<6), */ /* .dqspad_setting_override = 0, */ .lookup_table = { /* 0 - Quad Input/output read sequence - with optimised XIP support */ [0]=FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18), [1]=FLEXSPI_LUT_SEQ(MODE8_SDR, FLEXSPI_4PAD, 0xA0, DUMMY_SDR, FLEXSPI_4PAD, 0x04), [2]=FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_4PAD, 0x04, JMP_ON_CS, 0, 1), /* 1 - Read Status */ [1*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x01), /* 3 - Write Enable */ [3*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP, 0, 0), /* 4 - Write status */ [4*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x01, WRITE_SDR, FLEXSPI_1PAD, 0x1), /* 5 - Erase Sector */ [5*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD7, RADDR_SDR, FLEXSPI_1PAD, 0x18), /* 9 - Page Program */ [9*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x02, RADDR_SDR, FLEXSPI_1PAD, 0x18), [9*4+1] = FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x8, STOP, FLEXSPI_1PAD, 0x0), /* 11 - Chip Erase */ [11*4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xC7, STOP, FLEXSPI_1PAD, 0x0), }, }, .page_size = 256u, .sector_size = 4u * 1024u, .blocksize = 32u * 1024u, .is_uniform_blocksize = false, };__attribute__((section(".boot_hdr.ivt"))) const struct ivt_s g_image_vector_table = { IVT_HEADER, /* IVT Header */ 0x60002000, /* Image Entry Function */ IVT_RSVD, /* Reserved = 0 */ (uint32_t)DCD_ADDRESS, /* Address where DCD information is stored */ (uint32_t)BOOT_DATA_ADDRESS, /* Address where BOOT Data Structure is stored */ (uint32_t)&g_image_vector_table, /* Pointer to IVT Self (absolute address) */ (uint32_t)CSF_ADDRESS, /* Address where CSF file is stored */ IVT_RSVD /* Reserved = 0 */ }; __attribute__((section(".boot_hdr.boot_data"))) const struct boot_data_s g_boot_data = { FLASH_BASE, /* boot start location */ (FLASH_END - FLASH_BASE), /* size */ PLUGIN_FLAG, /* Plugin flag*/ 0xFFFFFFFF /* empty - extra data word */ };
Drop me a note if you want an image to just try burning into the chip to see if it will boot from it...you should be able to do that from JLinkExe which would at least put to bed any concern over hardware issues.
Regards
DAVE
Hi dmarples,
I see what you're on about with editing the boot header configuration... that does have to be customized to match the flash device that's in use on the board. Can you tell me what flash device you have on your RT1021 board? I need to reconcile some of what's in your source code with your device's datasheet. so I can better understand how to modify my code for our flash device. We're using a Cypress S25FL256L (datasheet), and I can see that its geometry and command set is slightly different from what you have defined.
David R.
I'm using the same devices as on the Eval Board, IS25LP064A. It's a while since I made the changes but IIRC you don't need _all_ of the entries in the boot header to bring it up (once I'd figured out the structure of the boot header, then it was easier to put them all in for the case I might need them later). I would recommend dropping one of these chips onto your board to remove a variable, then working back to your flash device.
Regards
DAVE
So your code was quite helpful in helping me understand what exactly is going on in the boot header. I can see how the code conforms to the ISSI IS25LP064, and also what needs to change for my Cypress S25FL256 device. Notably, the Cypress part has four status registers (well, one status and three configuration registers), and the QUAD enable bit is in bit 1 of the second register, not bit 3 of the first. So right now this is my boot header code:
/* Width of flash addresses (either 24 or 32). */
#define QSPI_ADDR_WIDTH 24u
#ifdef USE_QSPI
const flexspi_nor_config_t qspi_config = {
.memConfig = {
.tag = FLEXSPI_CFG_BLK_TAG,
.version = FLEXSPI_CFG_BLK_VERSION,
.readSampleClkSrc = kFlexSPIReadSampleClk_LoopbackInternally,
.csHoldTime = 3u,
.csSetupTime = 3u,
/* This defines the sequence to use to set the QUAD bit.
* Command 0x01 writes up to four registers - SR1V, CR1V, CR2V, CR3V.
* SR1V = 0x00 (no protection)
* CR1V = 0x20 (bit 1 = QUAD enable, all other bits to 0)
* CR2V = 0x60 (defaults -- high driver impedance, QPI off, 24-bit addresses)
* CR3V = 0x78 (defaults -- 64 byte wrap, wrap disabled, 8 read dummy cycles) */
.deviceModeCfgEnable = true,
.deviceModeSeq.seqNum = 1,
.deviceModeSeq.seqId = 4,
.deviceModeArg = 0x00026078,
/* Device geometry, I/O, and speed. */
.deviceType = kFlexSpiDeviceType_SerialNOR,
.sflashPadType = kSerialFlash_4Pads,
.serialClkFreq = kFlexSpiSerialClk_100MHz,
.sflashA1Size = 32u * 1024u * 1024u,
.dataValidTime = {16u, 16u},
/* Lookup table for flash commands for this device. Up to 8 instructions
* can be defined for each LUT table location. Each instruction is 16 bits,
* and the data structure organizes them as 32-bit words (for some reason). */
.lookupTable = {
/* 0 - Quad Input/output read sequence - with optimized XIP support */
[0*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB,
RADDR_SDR, FLEXSPI_4PAD, QSPI_ADDR_WIDTH),
[0*4+1] = FLEXSPI_LUT_SEQ(MODE8_SDR, FLEXSPI_4PAD, 0xA0, // 2 dummy cycles
DUMMY_SDR, FLEXSPI_4PAD, 4), // 4 dummy cycles
[0*4+2] = FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_4PAD, 4,
JMP_ON_CS, FLEXSPI_1PAD, 1),
/* 1 - Read Status */
[1*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05,
READ_SDR, FLEXSPI_1PAD, 1), // Read 1 byte
/* 3 - Write Enable */
[3*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06,
STOP, FLEXSPI_1PAD, 0),
/* 4 - Write status */
[4*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x01,
WRITE_SDR, FLEXSPI_1PAD, 4), // Write 4 bytes
/* 5 - Erase Sector */
[5*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD8, // Block Erase
RADDR_SDR, FLEXSPI_1PAD, QSPI_ADDR_WIDTH),
/* 9 - Page Program */
[9*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x02,
RADDR_SDR, FLEXSPI_1PAD, QSPI_ADDR_WIDTH),
[9*4+1] = FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x08,
STOP, FLEXSPI_1PAD, 0),
/* 11 - Chip Erase */
[11*4+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xC7,
STOP, FLEXSPI_1PAD, 0x0),
},
},
/* Pretend that our sectors (4KB) are as big as our 64KB blocks. */
.pageSize = 256u,
.sectorSize = 64u * 1024u,
.blockSize = 64u * 1024u,
.isUniformBlockSize = true,
};
#else
const flexspi_nor_config_t hyperflash_config = {
[...]
};
#endif // USE_QSPI
I'm not sure if this is completely correct, but it seems that the boot utility liked it enough to flash my SREC image to my board. I think what I probably need to do now is verify that I have an actual functioning target by loading code into RAM, then maybe probe SDRAM to verify that's functioning, then try loading code into flash again.
It's not trivial to swap flash devices on this board... it's an 8-WSON package. I don't have reason to question the flash device right now; I've got a number of other things to investigate before I try swapping chips. You've been quite helpful, thanks.
David R.
Dave,
Are you using a Quad SPI Flash that is different from the IS25WP064A populated on the EVK?
Can you comment on the changes you made to the flash config structure that differ from those listed in this thread?
Thanks
I've provided several screenshots above, showing QSPI bus activity, the behavior of the SEGGER programming window, the debugger context when the debug session launches, and the error dialog when I try programming the board directly using MCU Boot Utility.
I'll provide a summary of my configuration and my issues here:
Can you provide any assistance for these issues?
Hi David Rodgers,
Thanks a lot for your detail information.
In factor, the secondary pin mux option connect to the nor flash, not only related to the BOOT_CFG, BOOT_MODE configuration, you also need to configure the option0 and option1 in the flashloader, that's why you have problems both in the mcuxpresso IDE and MCUBootutility.
About the MCUXpresso IDE associated with JLINK, it may need to modify some files in the JLINK driver. Actually, if you are using the IAR, it will be more easy to modify it, you can modify the .board files.
But, about the MCUBootUtility tools, I have checked it with the tool author yesterday, but forget to tell you the details, now, please use the MCUbootUtility to download the code again.
1. RT board enter the serial download mode, BOOT_MODE=01.
2. Open the MCUBootUtility tool, configure the following point:
option 0[Has option1]=1, option1[enable second pinmux] =1, just choose the secondary pin mux.
Then, when you download the code, the flashloader will try the nor flash which is connect to the secorday mux pins.
Please try it on your side.
Any updated information, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Finally coming back around to try and get this working... regarding the MCU Boot Utility, I did modify my Boot Device Configuration to select "Has Option1" and "Enable Second Pinmux", but I'm still getting the error dialog that says
Bootable image is not generated successfully! Make sure you don't put the tool in path with blank space!
See my comment above where I detailed what was occurring. I've attached a text file (anonymized) of the output of the console window when I hit the "All-in-One Action" button. You can see from the output that I have the tool installed in a space-free directory path. Any ideas what's wrong with the Boot Utility?
For the error "Bootable image is not generated...", Can you please try to use srec/hex file instead of .axf file?
It seems that ROM/Flashloader can access NOR Flash via second pinmux properly,You can connect to NOR device by MCUBootUtility, right?
Hi jayheng,
It appears I've achieved some level of success with the MCU Boot Utility. I don't have a working target yet, but it appears that the utility is now doing what it's supposed to be doing. After some investigation, I determined that I needed to make one more setting change for my Cypress S25FL256 device, to select "Set StatusReg2[1]" for Quad Mode:
I did also add a post-build step to generate an SREC file instead, and that seemed to make the tool much happier. It passed the phase of generating the bootable file (in the log, the tool says "Origianl image file is a bootable image file"), then spent almost two minutes sending the image to the target. The utility finished with a stopped clock looking like this:
And now when I do an internal boot, I see a much different pattern on the logic analyzer:
This is strongly suggesting to me that I have in fact programmed the flash on my board. So now I need to turn my attention to getting the debugger to push a useful image into my target hardware.
David R.
For the reason that you need addtional setting "Set StatusReg2[1]" for Cypress S25FL256, I believe this NOR device is not compatible with JESD216A/B/C.
For the reason that MCUBootUtility spent two minutes flashing image, actually, most of the time is used to readback the image from device, you can disable image readback by setting 'Tools/Image Readback' to 'Manual' in menu bar.
In a word, You can use MCUBootUtility properly now, i believe you can enable FlexSPI NOR boot on secondary pinmux in your board as well.
I'm not aware of any need to change files in jlink, at least for the
1021...it may of course be different for the other chips. There is a need
to change jlink files when you're moving from hyperflash to qspi (there is
jlink documentation available on this) but not according to which bus
you've got your qpsi device connected to - provided you've not messed with
the fuses then that is set by the configuration pins.
Regards
Dave
Hi Austin Wilhite,
Please check my attached JLinkDevices.xml, it modify the RT105X from hyper flash to QSPI flash.
Wish it helps you!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi kerryzhou,
I can see in the modified XML file that J-Link is being told to use the QSPI driver instead of the HyperFlash driver when selecting an RT1050. I guess my next question is... why are we forced to hack a J-Link configuration file to make this work? Shouldn't there be multiple options when selecting the CPU, to choose whether HyperFlash or QSPI flash is in use? Has anyone from NXP coordinated with SEGGER on this issue? It shouldn't be necessary to hack the development tools to flash program a device. Now I have to swap XML files back and forth when switching between my RT1050 EVKB and my RT1050 target hardware board.
I did try to use the above XML file changes to program my board... the behavior is different from the previous configuration, but the board still does not program correctly. I see the Compare bar grow in small increments to 100%, then the Erase bar grows to 100%, then the SEGGER programming window closes, then a new one opens, the Compare bar quickly grows to 100%, then the Erase bar grows to 100%, then that window closes, and the debugger drops somewhere into the ROM.
David R.
Hi David Rodgers,
This is really not very convenient to modify the xml files, it seems when use the JLINK with Fflash or the MCUXpresso IDE need to modify that file. But if you use the CMSIS DAP debugger or other IDE, you don't modify the install path data, because the official already provide the related files.
Because your board is the customer board, do you try to download the code to the internal RAM, whether it works OK or not, just make sure your smallest system has no problem at first, you also can try to test the SDK flexspi_nor_polling project, but you need to modify the flexIO pins, test whether you can read/write the external flash memory successfully? Then we can make sure the problem is in the secondary pin mux flash memory side.
I still don't have the hardware to connect to the secondary pinmux pins, so I don't have the hardware condition to test it directly now.
Could you use the IAR project, test this SDK code in RAM at first?
SDK_2.6.1_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\flexspi\nor\polling_transfer\iar
Please modfy the pinmux.c change the flexSPI pins to your own flash related pins.
If the flash operation works OK, then we can find a simple code, eg, led_blinky, modify the .board(actually configure opt0 and opt1), just use the IAR IDE with JLINK debugger try it again, not use the mcuxpresso IDE at first.
Any test result please kindly let me know.
Wish it helps you!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Dave Marples,
You are right, the JLINK file which is needed to mofiy is the JLinkDevices.xml file, as you know, the default setting is used for Hyper Flash.
The option0 and option1 is used when download the code with MCUBootUtility, it is used to select the secondary pin mux.
Could you tell me your RT1020 with JLINK is based on which IDE? MCUXPresso or others, eg IAR, MDK?
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------